This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Davinci Bringup Problem

Hi,

I am tring to bringup DM64x Davinci board, but its not working, Here is the log for same

DVPB #boot
BOOTP broadcast 1
DHCP client bound to address 10.110.1.133
TFTP from server 10.110.0.19; our IP address is 10.110.1.133
Filename 'pxelinux.bin'.
Load address: 0x80700000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ######################################################
done
Bytes transferred = 1935912 (1d8a28 hex)
## Booting image at 80700000 ...
   Image Name:   Linux-2.6.32-rc2-davinci1
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1935848 Bytes =  1.8 MB
   Load Address: 80700000
   Entry Point:  80700000
   Verifying Checksum ... OK
   XIP Kernel Image ... OK

Starting kernel ...


:: and it stuck at this position, Please give me some solution for same...

Thanks
Tushar P