This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error while booting



Hi,

I get a --->  TimeOut occured in boot_proc

                    program exit

This is a part of the boot up . This error comes while booting  camera which uses DM365 processor. Why does this boot proc error  come ?

Have made that error bold.

Starting internet superserver: inetd.
io scheduler deadline registered
io scheduler cfq registered
i2c_emac: disagrees about version of symbol struct_module
insmod:  sbulla:cannot insert `/ unknown partition table
opt/ipnc/modules/i2c-emac.ko': Invalid module format (-1): Exec format error
Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
loop: loaded (max 8 devices)
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
CSLIP: code copyright 1989 Regents of the University of California
netconsole: disagrees about version of symbol struct_module
PPP generic driver version 2.4.2
insmod: cannot insert `/opt/ipnc/modules/netconsole.ko': Invalid module format (-1): Exec format error
PPP Deflate Compression module registered
davinci_emac: disagrees about version of symbol struct_module
mmc_core: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/davinci_emac.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/mmc_core.ko': Invalid module format (-1): Exec format error
mmc_block: disagrees about version of symbol struct_module
davinci_mmc: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/mmc_block.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/davinci-mmc.ko': Invalid module format (-1): Exec format error
usbcore: disagrees about version of symbol struct_module
musb_hdrc: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/usbcore.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/musb_hdrc.ko': Invalid module format (-1): Exec format error
usbmon: disagrees about version of symbol struct_module
Loading iSCSI transport class v1.1-646.insmod: cannot insert `/opt/ipnc/modules/usbmon.ko': Invalid module format (-1): Exec format error
<5>iscsi: registered transport (tcp)
 sbulla: unknown partition table
mkdosfs 3.0.6 (04 Oct 2009)
unable to get drive geometry, using default 255/63
/dev/sbulla has 255 heads and 63 sectors per track,
logical sector size is 512,
using 0xf8 media descriptor, with 1024 sectors;
file system has 2 12-bit FATs and 4 sectors per cluster.
FAT size is 1 sector, and provides 247 clusters.
Root directory contains 512 slots.
Volume ID is b1604dfa, no volume label.
queue id:0
umount: /mnt/mmc: not mounted
killall: dhcpcd: no process killed
TimeOut occure in boot_proc.
Program exit.