This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 uboot: nand speed is very low?

When i use nand write or nand read In my board (DM8148 EVM), the speed of operation is very low !

But if i come into kernel, the nand speed get well !

So, how to speed the nand operation in uboot ? I have made many change but is useless.

  • hi Jiangao,

    Could you please provide more details? What command for nand read you are using? I just try this on my own DM8148 EVM:

    TI8148_EVM# nand read 0x80000000 0x400000 0x400000

    And it works for less than a second:

    NAND read: device 0 offset 0x400000, size 0x40000
     262144 bytes read: OK

    Best regards,

    Pavel

  • TI8148_EVM#nandecc hw 0
    HW ECC Hamming Code selected
    TI8148_EVM#nand read 81000000 400000 400000

    NAND read: device 0 offset 0x400000, size 0x400000
     4194304 bytes read: OK
    TI8148_EVM#

     

    it takes about 7 seconds, it's too slow.

    My uboot: u-boot-2010.06-psp04.01.00.06

  • hi Jiangao,

    When I try TI8148_EVM#nand read 81000000 400000 400000, it takes about 3 seconds. And I am with the newest u-boot: u-boot-2010.06-psp04.04.00.01. This u-boot is available in the new DM814x EZSDK 5.04.00.11. Could you please try with the new u-boot.

    Best regards,

    Pavel

  • I will have a try and let you know.

    But, 1M/s is remain a low speed, there is any way to speed up it ?

    thanks.

     

  • Hi Jiangao,

    As you said that in the kernel your speed is fine, could you please provide me the following parameters values from your kernel:

    1. The main CPU (Cortex-A8 ARM) clock frequency - arm_dpll_clk

    2. The GPMC module clock frequency - gpmc_fclk

    3. The GPMC_CONFIGx_0 (x = 1 to 7) registers values

    Meanwhile, you can try to speed up the NAND operations through increasing the main CPU and GPMC module clock frequencies to 1000 MHz and 130 MHz.

    Best regards,

    Pavel

  • some information in my kernel:

    gpmc_fck:      100000000

    arm_dpll_ck: 600000000

    mpu_ck:         600000000

    GPMC_CONFIG1_0(d0804060) = 810
    GPMC_CONFIG2_0(d0804064) = 1e1e00
    GPMC_CONFIG3_0(d0804068) = 1e1e00
    GPMC_CONFIG4_0(d080406c) = 16051807
    GPMC_CONFIG5_0(d0804070) = 151e1e
    GPMC_CONFIG6_0(d0804074) = 16000f80
    GPMC_CONFIG7_0(d0804078) = 48

    some info on my uboot:

    U-Boot 2010.06 (Jun 09 2012 - 09:58:39)

    TI8148-GP rev 2.1

    ARM clk: 600MHz
    DDR clk: 400MHz

    DRAM:  2 GiB
    NAND:  HW ECC BCH8 Selected

     

     

    I test the nand speed use mtd_speedtest:

    mtd_speedtest: testing eraseblock write speed
    mtd_speedtest: eraseblock write speed is 1854 KiB/s
    mtd_speedtest: testing eraseblock read speed


    mtd_speedtest: eraseblock read speed is 2252 KiB/s
    mtd_speedtest: testing page write speed

    mtd_speedtest: page write speed is 1854 KiB/s
    mtd_speedtest: testing page read speed

     

    So, it looks like the nand speed in kernel is not fast !

    my question:

     1: 2M/s is a normal speed?

     2: How to speed up it ?

  • This is a mtd speed test of my another platform: (MLC, Hynix2GB)

    [   40.070000]
    [   40.070000] =================================================
    [   40.072000] mtd_speedtest: MTD device: 4
    [   40.076000] mtd_speedtest: MTD device size 16777216, eraseblock size 2097152, page size 8192, count of eraseblocks 8, pages per eraseblock 256, OOB size 448

    [   40.345000] mtd_speedtest: scanning for bad eraseblocks
    [   40.378000] mtd_speedtest: scanned 8 eraseblocks, 0 are bad
    [   40.458000] mtd_speedtest: testing eraseblock write speed
    [   44.870000] mtd_speedtest: eraseblock write speed is 3713 KiB/s
    [   44.870000] mtd_speedtest: testing eraseblock read speed
    [   46.220000] mtd_speedtest: eraseblock read speed is 12190 KiB/s
    [   46.275000] mtd_speedtest: testing page write speed

    [   54.200000] mtd_speedtest: page write speed is 2067 KiB/s
    [   54.200000] mtd_speedtest: testing page read speed
    [   55.374000] mtd_speedtest: page read speed is 14003 KiB/s
    [   55.395000] mtd_speedtest: testing 2 page write speed

    [   59.346000] mtd_speedtest: 2 page write speed is 4146 KiB/s
    [   59.346000] mtd_speedtest: testing 2 page read speed
    [   60.548000] mtd_speedtest: 2 page read speed is 13721 KiB/s
    [   60.548000] mtd_speedtest: Testing erase speed
    [   60.573000] mtd_speedtest: erase speed is 819200 KiB/s
    [   60.573000] mtd_speedtest: finished
    [   60.576000] =================================================
    #

    [   46.220000] mtd_speedtest: eraseblock read speed is 12190 KiB/s !

    so , it is necessary to improve the dm8148 nand speed now.

  • Hi Jiangao,

    We can try to speed up with increasing the CPU clock frequency (600 -> 1000 MHz) and GPMC clock frequency (100 -> 130 MHz).

    1. To increase the CPU clock frequency, modify in file ${EZSDK}/board-support/u-boot-2010.06-psp04.04.00.01/arch/arm/include/asm/arch-ti81xx/clocks_ti814x.h, parameter MODENA_M to 0x64:

    //#define MODENA_M    0x3C

    #define MODENA_M    0x64

    2. To increase the GPMC clock frequency, modify in file ${EZSDK}/board-support/u-boot-2010.06-psp04.04.00.01/arch/arm/include/asm/arch-ti81xx/clocks_ti814x.h, parameter L3_M to 1040:

    //#define L3_M        (pg_val_ti814x(880, 800))

    #define L3_M        (pg_val_ti814x(880, 1040))

    Best regards,

    Pavel

  • I have made some change in uboot:

    #define MODENA_N 0x1
    #define MODENA_M 0x64//0x3c//0x64
    #define MODENA_M2 1
    #define MODENA_CLKCTRL 0x1

    #define L3_N  19
    #define L3_M  (pg_val_ti814x(880, 1040/*800*/))
    #define L3_M2  4
    #define L3_CLKCTRL 0x801

    #define DDR_N  19
    #define DDR_M  (pg_val_ti814x(666, 800))
    #define DDR_M2  2
    #define DDR_CLKCTRL 0x801

    #define DSP_N  19
    #define DSP_M  750//500//750
    #define DSP_M2  1
    #define DSP_CLKCTRL 0x801

     

    And this the uboot output:

    U-Boot 2010.06 (Jun 12 2012 - 08:34:37)

    TI8148-GP rev 2.1

    ARM clk: 1000MHz
    DDR clk: 400MHz

    I2C:   ready
    DRAM:  2 GiB
    NAND:  HW ECC BCH8 Selected
    nand dev_id = d3

     

    Result:

    i use "nand read 81000000 1000000 a00000" in uboot, and it takes almost 16 seconds !

    TI8148_EVM#nand read 81000000 1000000 a00000

    NAND read: device 0 offset 0x1000000, size 0xa00000
    Skipping bad block 0x01360000
     10485760 bytes read: OK
    TI8148_EVM#

     

    So, is there another way to speed up it ?

     

    Thank you very mush !

  • Hi Jiangao,

    When I try this command: TI8148_EVM#nand read 81000000 1000000 a00000

    I have this result:

    TI8148_EVM#nand read 81000000 1000000 a00000

    NAND read: device 0 offset 0x1000000, size 0xa00000
     10485760 bytes read: OK
    TI8148_EVM#

    And it takes about 5 seconds! What should we do now is to improve your GPMC module timing parameters:

    GPMC_CONFIG1_0 = 1810
    GPMC_CONFIG2_0 = 40400
    GPMC_CONFIG3_0 = 40301
    GPMC_CONFIG4_0 = 3010501
    GPMC_CONFIG5_0 = 50707
    GPMC_CONFIG6_0 = 16000f80
    GPMC_CONFIG7_0 = f48

    Please update your GPMC_CONFIGx_0 registers with the values above.

    Best regards,

    Pavel


  • Ok, the speed is remain not In my expectations。

    But thank you very much !

  • Jiangao & Pavel,

    We've achieved around 8MB/sec throughput in DM8148EVM for NAND read. Please get in touch if you need a better solution. My mail id is renjith.thomas@pathpartnertech.com

  • Hi Renjith,

    Could you please post here the following:

    1. Your CPU clock frequency

    2. Your GPMC fclk frequency

    3. Is your NAND memory attached to CS0? If yes, please provide your GPMC_CONFIGx_0 (x = 1 to 7) registers settings

    4. Is your NAND memory from Micron? If yes, what is the chip id?

    Thanks,

    Pavel

  • Pavel,

    I made a mistake here, this was done on DM8168EVM and not on 8148. But GPMC is almost same. Please find the answers below.

    1. ARM running @ 1GHz.

    2. GPMC frequency we didn't change, whatever is set default by u-boot.

    3. Its attached to CS0, as its EVM.

    4. The NAND part on Netra EVM is Mircon MT29F2G16AADWP.

  • Hi Renjith,

    Thanks for your answer.

    One more thing, could you please give us your GPMC_CONFIGx_0 (x = 1 to 7) registers values?

    For example, our values are:

    GPMC_CONFIG1_0 = 1810
    GPMC_CONFIG2_0 = 40400
    GPMC_CONFIG3_0 = 40301
    GPMC_CONFIG4_0 = 3010501
    GPMC_CONFIG5_0 = 50707
    GPMC_CONFIG6_0 = 16000f80
    GPMC_CONFIG7_0 = f48

    I want to verify that we are using the same.

    Best regards,

    Pavel

  • Pavel,

    My timings are for Netra EVM and not for Centaurus. Still you can give it a shot

    GPMC_CONFIG1 0x01001800
    GPMC_CONFIG2 0x00000400
    GPMC_CONFIG3 0x00160100
    GPMC_CONFIG4 0x01000000
    GPMC_CONFIG5 0x00031703
    GPMC_CONFIG6 0x00000000
    GPMC_CONFIG7 0x00000f48

  • Hi Renjith,

    I tried with these, but there is no speed-up progress. May be these are valid only for Netra EVM.

    When reading from NAND, are you using nandecc hw 0 (HW ECC Hamming Code)?

    One last thing that I can try is to align my rest GPMC registers values with yours. So I need these registers values that you are using:GPMC_CONFIG, GPMC_STATUS, GPMC_PREFETCH_CONFIG1, GPMC_PREFETCH_CONFIG2, GPMC_PREFETCH_CONTROL, GPMC_ECC_CONFIG, GPMC_ECC_CONTROL, GPMC_ECC_SIZE_CONFIG, GPMC_BCH_SWDATA

    Best regards,

    Pavel

  • Pavel,

    I dont think these changes are going to give you much gain. The problem lies not just in these register settings. You've to change the driver code to a certain extent. I'm afraid I'll not be able to disclose our optimization over the forum.

  • Hi pavel,

    On what basis have you changed the register values of GPMC_CONFIG registers.

    I see that according to the values suggested by you will change the number of GPMC_FCLK cycles.How are you calculating the GPMC_FCLK cycles?

    For example: My current GPMC_FCLK2_0 value is 1e1e00 and the value suggested by you is 40400. When we decode this value, the De-assertion time from start cycle to read (bit[8] to bit[12]) is 4 GPMC_FCLK cycle. Can you please let me know how you are calculating the number of GPMC_FCLK cycles for different access?

    Thanks in advance.

    Regards

    Prakash

  • Hi Prakash,

    I changed the registers values of GPMC_CONFIG registers, based on the fact that in u-boot we have one set of settings, and in linux kernel we have other set of settings. I did not made any calculations for the GPMC_FCLK cycles. The reported issue was that in u-boot, the NAND read/write speed is slow, while in kernel, NAND speed is well. So what I did is to compare the settings in GPMC in kernel, and apply these into u-boot. Then the speed in u-boot get well also.

    For how to calculate the GPMC_FCLK cycles, you can check here:

    1. DM814x TRM, chapter 11 GPMC, section 11.2.4.9 Timing Setting, section 11.3.6 GPMC Timing Parameters, 11.4.1 How to Set GPMC Timing Parameters for Typical Accesses

    2. http://processors.wiki.ti.com/index.php/Tips_for_configuring_OMAP35x,_AM35x,_and_AM-DM37x_GPMC_registers

    Regards,

    Pavel




  • Hi pavel,

    Thanks for your reply.

    Could you let me know in which file in the kernel the GPMC_CONFIGi registers are present?

    We are using 'micron NAND' and i am not able to find the GPMC_CONFIG registers to change their values suggested by you above.

    Thanks

    Prakash

  • Does anybody have any results with this problem?

    We face to the same issue in u-boot. GPMC works with NAND flash very slow. We discovered that there is a long time between sequential read cycles during nand reading operation. The time when CS is inactive about 800ns. I couldn`t reduce this time. Any changing the CPMC_CONFIG settings do not affect.

    It seems u-boot works quite slow in general, because we notice that ethernet works slower too in u-boot than in kernel.

  • Hi Evgeny,

    Which version of the EZSDK you are using? Make sure you are using the latest one 5.05

    You can check here also, for the expected performance:

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_04.04.00.01_Feature_Performance_Guide#NAND_Driver

    Regards,

    Pavel

  • Hi Pavel.

    Thank you for reply.

    We are using the latest version EZSDK 5.05.
    Your reference refer to NAND performance in kernel. I the kernel NAND flash works quite fast.
    I want to drow your attention that the problem with NAND performance in u-boot.

    Some additional information. In our device we are using Samsung SLC NAND Flash (8bit data bus).

    Best Regards, Evgeny Kvashnin.

  • Evgeny,

    You can optimize the NAND driver in u-boot to get good speeds of the range 10MB/sec.