This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

reduce booting time about ti8168



Hello everyone,

It takes about 1 minute when booting up with SD card on my ti8168 board,(Too long)

and I want to reduce it to about 30seconds or less. Is it possible?

I found it always takes long time at 

            [ 1.580000] EXT3-fs: barriers not enabled

and

            Remounting root file system...

Is there any advises about this problem? Thank you.

BTW,This is the log about the SD boot.

U-Boot 2010.06 (May 23 2012 - 14:40:14)

DRAM: 2 GiB
Using default environment

Hit any key to stop autoboot: 0
mmc1 is available
reading u-boot.bin

179356 bytes read
## Starting application at 0x80800000 ...


U-Boot 2010.06 (May 23 2012 - 14:40:41)

TI8168-GP rev 1.1

ARM clk: 987MHz
DDR clk: 398MHz

I2C: ready
DRAM: 2 GiB
NAND: HW ECC Hamming Code selected
No NAND device found!!!
0 MiB
*** Warning - bad CRC or NAND, using default environment

:,;;:;:;;;;;;;;r;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:;;;;;;;;:,;;:;:
;,;:::;;;;r;;;rssiSiS552X5252525259GX2X9hX9X9XX2325S55252i5:,;;:;:;;;;;;;;:,;;:
;:;;;;;;;rrssSsS52S22h52299GGAAMHMM#BBH#B#HMM#HMBA&&XX2255S2S5Si:,;;:;:;;;;;;;;
;:;;r;;rsrrriiXS5S329&A&MH#BMB#A&9XXA252GXiSXX39AAMMMBB&G22S5i2SSiiiisi:,;;:;:;
;;;;;r;rr2iisiih393HB#B#AA99i22irrrX3X52AGsisss2Xii2299HBMA&X2S5S5iSiisSsi:,;;:
r:r;rrsrsihXSi2&##MHB&Ahh3AGHGA9G9h&#H##@@@##MAMMXXX9SSS29&&HGGX2i5iisiiisisi:,
;;rrrrsSiiiA&ABH&A9GAGhAhBAMHA9HM@@@@@@@@@@@@@@@@@@@HHhAh2S2SX9&Gh22SSiisiiisii
r:rrssisiS2XM##&h3AGAX&3GG3Ssr5H@M#HM2; ;2X&&&MHMB###GBB#B&XXSSs529XX55iSsisisi
r;rsrisSi2XHAhX99A3XXG&&XS;:,rH#HGhAS @@@@3rs2XBM@@A552&&AHA2XiisSS252SSsisSs
r;issi5S22&&3iSSX292&hXsr;;:;h@&G339&S9@@@@2@MA&9&HB##Xris29ABMAAX2ir;rsSi5iss5
rrsSi2XhG&9GXh399&X99i;;;;;;r#H&293H9X#@@@@@@@B&9GhAH@XrrsrsiXABHB&HG2rr;rrSiSi
;:rsisS599&AA9XG&3A35r;:::;,;BMh&&2iX5A@@@@@@@&392X5GB2;;;r;iSX393A##A&Xi:::rsi
;:rss552222X553&XHMhir;;::,:,h#HhGSXhG3#@@@@#AXXS2XAHA;::;;;;ss55XShBA3239r:,;;
r;ii2S5SSi2i53hirsh2srr::,,,,;MMXX359&Ah3h&Si59SX99A#i:,::::;;sri2,.2r;:SGAr;,:
;:;rrrrssiriXGSi::shs;;;,,,:,,rBBA9h5s5h5iS5isi2SAHB5:,,,:::;rrs5&SrisSX5Srrr:,
;,r;;;;rsriSSrrrr;;5Xrr;;,:,,.,;9AA2SsisS5323XXXG9&i:.,,::;;r;;;srrrrrr;;:;::::
:,;r;r;rrissrrr;:;::;s;;;;,:,,..,r293h222hXXAAGGGX;:,,,:,:,::;:;::,:,,,,...,,,,
;,;;;;rrrrrrrrirr;,.,,:::::::,,,,.,;SX&ABAB2hhXir:,,.,,.,,:,,,,..,,,..,..,,,..:
:.:;:;;;:;;;;r;rrs;:.. ,,:::::,:,:,,.::rrsrr;;,,.......,..,....,,,,,,,...,.,,:,
:.:::,::::::;;r;rrr;:.......,.,.,,:::,,...............,,::.,,,,:,::,,:,:,,,:,;:
,.::,:,,,,,;;;;;;;;r;;::,..............................;;;:;::::,:::::::,:,:,,,
: ,,:,,,,,,,,,,,,,:;rrr;;:;,,,,,,,::,.,.:.,.,;s,:;;;;:;:;;;;;::::,:::,:::,:,:,:
,.,,,,,,,...,,.,,....................................:,............:,,,:,:,,,,,

Net: <ethaddr> not set. Reading from E-fuse
Detected MACID:90:d7:eb:2d:1e:ca
Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot: 3 2 1 0
mmc1 is available
reading boot.scr

300 bytes read
Running bootscript from MMC/SD to set the ENV...
## Executing script at 80900000
reading uImage

1955080 bytes read
## Booting kernel from Legacy Image at 80009000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1955016 Bytes = 1.9 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 2.6.37 (xiaoxiao@ubuntu) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #3 Wed May 30 11:50:16 JST 2012
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: ti8168evm
[ 0.000000] vram size = 52428800 at 0
[ 0.000000] reserved size = 52428800 at 0
[ 0.000000] FB: Reserving 52428800 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] OMAP chip is TI8168 1.1
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 52224
[ 0.000000] Kernel command line: console=ttyO2,115200n8 rootwait root=/dev/mmcblk0p2 rw mem=256M earlyprink notifyk.vpssm3_sva=0xBF900000 vram=50M ti816xfb.vram=0:16M,1:16M,2:6M ip=off noinitrd
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 206MB = 206MB total
[ 0.000000] Memory: 204436k/204436k available, 57708k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
[ 0.000000] vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc0033000 ( 172 kB)
[ 0.000000] .text : 0xc0033000 - 0xc03b2000 (3580 kB)
[ 0.000000] .data : 0xc03b2000 - 0xc03ee480 ( 242 kB)
[ 0.000000] SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] NR_IRQS:407
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] GPMC revision 6.0
[ 0.000000] Trying to install interrupt handler for IRQ400
[ 0.000000] Trying to install interrupt handler for IRQ401
[ 0.000000] Trying to install interrupt handler for IRQ402
[ 0.000000] Trying to install interrupt handler for IRQ403
[ 0.000000] Trying to install interrupt handler for IRQ404
[ 0.000000] Trying to install interrupt handler for IRQ405
[ 0.000000] Trying to install interrupt handler for IRQ406
[ 0.000000] Trying to install type control for IRQ407
[ 0.000000] Trying to set irq flags for IRQ407
[ 0.000000] OMAP clockevent source: GPTIMER1 at 27000000 Hz
[ 0.000000] Console: colour dummy device 80x30
[ 0.000000] Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
[ 0.240000] pid_max: default: 32768 minimum: 301
[ 0.250000] Security Framework initialized
[ 0.250000] Mount-cache hash table entries: 512
[ 0.250000] CPU: Testing write buffer coherency: ok
[ 0.250000] devtmpfs: initialized
[ 0.250000] omap_voltage_early_init: voltage driver support not added
[ 0.250000] regulator: core version 0.5
[ 0.250000] regulator: dummy:
[ 0.250000] NET: Registered protocol family 16
[ 0.250000] OMAP GPIO hardware version 0.1
[ 0.250000] OMAP GPIO hardware version 0.1
[ 0.250000] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.250000] _omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
[ 0.250000] _omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
[ 0.250000] NOR: Can't request GPMC CS
[ 0.250000] registered ti816x_vpss device
[ 0.250000] registered ti816x_gpio_vr device
[ 0.250000] registered TI816x on-chip HDMI device
[ 0.250000] registered ti816x_sr device
[ 0.250000] pm_dbg_init: only OMAP3 supported
[ 0.250000] Registered ti81xx_fb device
[ 0.250000] ti816x_pcie: Invoking PCI BIOS...
[ 0.250000] ti816x_pcie: Setting up Host Controller...
[ 0.250000] ti816x_pcie: Register base mapped @0xd0820000
[ 0.360000] ti816x_pcie: Starting PCI scan...
[ 0.360000] PCI: bus0: Fast back to back transfers enabled
[ 0.360000] bio: create slab <bio-0> at 0
[ 0.360000] regulator: VFB: 800 <--> 1025 mV at 800 mV
[ 0.360000] vgaarb: loaded
[ 0.360000] usbcore: registered new interface driver usbfs
[ 0.360000] usbcore: registered new interface driver hub
[ 0.360000] usbcore: registered new device driver usb
[ 0.360000] omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
[ 0.380000] omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz
[ 0.380000] Switching to clocksource gp timer
[ 0.380000] musb-hdrc: version 6.0, host, debug=0
[ 0.380000] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.400000] registerd cppi-dma Intr @ IRQ 17
[ 0.400000] Cppi41 Init Done
[ 0.400000] musb-hdrc: kernel must blacklist external hubs
[ 0.400000] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 0.400000] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
[ 0.400000] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.400000] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.400000] usb usb1: Product: MUSB HDRC host driver
[ 0.400000] usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
[ 0.400000] usb usb1: SerialNumber: musb-hdrc.0
[ 0.400000] hub 1-0:1.0: USB hub found
[ 0.400000] hub 1-0:1.0: 1 port detected
[ 0.400000] musb-hdrc musb-hdrc.0: USB Host mode controller at d080c000 using DMA, IRQ 18
[ 0.400000] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.420000] musb-hdrc: kernel must blacklist external hubs
[ 0.420000] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.420000] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
[ 0.420000] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.420000] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.420000] usb usb2: Product: MUSB HDRC host driver
[ 0.420000] usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
[ 0.420000] usb usb2: SerialNumber: musb-hdrc.1
[ 0.420000] hub 2-0:1.0: USB hub found
[ 0.420000] hub 2-0:1.0: 1 port detected
[ 0.420000] musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using DMA, IRQ 19
[ 0.420000] NET: Registered protocol family 2
[ 0.420000] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.420000] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.420000] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.420000] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.420000] TCP reno registered
[ 0.420000] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.420000] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.420000] NET: Registered protocol family 1
[ 0.420000] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.420000] PMU: registered new PMU device of type 0
[ 0.420000] omap-iommu omap-iommu.0: ducati registered
[ 0.420000] omap-iommu omap-iommu.1: sys registered
[ 0.490000] JFFS2 version 2.2. (NAND) ツゥ 2001-2006 Red Hat, Inc.
[ 0.490000] msgmni has been set to 399
[ 0.490000] io scheduler noop registered
[ 0.490000] io scheduler deadline registered
[ 0.490000] io scheduler cfq registered (default)
[ 0.490000] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.490000] omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
[ 0.490000] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.490000] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 1.200000] console [ttyO2] enabled
[ 1.210000] brd: module loaded
[ 1.220000] loop: module loaded
[ 1.220000] m25p80 spi1.0: found m25p32, expected w25x32
[ 1.230000] m25p80 spi1.0: m25p32 (4096 Kbytes)
[ 1.230000] Creating 4 MTD partitions on "spi_flash":
[ 1.240000] 0x000000000000-0x000000040000 : "U-Boot"
[ 1.240000] 0x000000040000-0x000000042000 : "U-Boot Env"
[ 1.250000] mtd: partition "U-Boot Env" doesn't end on an erase block -- force read-only
[ 1.260000] 0x000000042000-0x0000002c2000 : "Kernel"
[ 1.260000] mtd: partition "Kernel" doesn't start on an erase block boundary -- force read-only
[ 1.270000] 0x0000002c2000-0x000000400000 : "File System"
[ 1.280000] mtd: partition "File System" doesn't start on an erase block boundary -- force read-only
[ 1.290000] omap2-nand driver initializing
[ 1.290000] No NAND device found.
[ 1.300000] No NAND device found.
[ 1.350000] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.350000] davinci_mdio davinci_mdio.0: detected phy mask fffffffd
[ 1.360000] davinci_mdio.0: probed
[ 1.360000] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
[ 1.370000] usbcore: registered new interface driver cdc_ether
[ 1.380000] usbcore: registered new interface driver dm9601
[ 1.380000] mice: PS/2 mouse device common for all mice
[ 1.390000] i2c /dev entries driver
[ 1.390000] Linux video capture interface: v2.00
[ 1.400000] usbcore: registered new interface driver uvcvideo
[ 1.400000] USB Video Class driver (v1.0.0)
[ 1.410000] OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
[ 1.410000] usbcore: registered new interface driver usbhid
[ 1.420000] usbhid: USB HID core driver
[ 1.420000] notify_init : notify drivercreated for remote proc id 2 at physical Address 0xbf900000
[ 1.430000] TCP cubic registered
[ 1.440000] NET: Registered protocol family 17
[ 1.440000] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.450000] omap_voltage_late_init: Voltage driver support not added
[ 1.460000] smartreflex smartreflex: Driver initialized
[ 1.470000] Waiting for root device /dev/mmcblk0p2...
[ 1.540000] mmc0: new high speed SDHC card at address 1234
[ 1.540000] mmcblk0: mmc0:1234 SA04G 3.63 GiB
[ 1.550000] mmcblk0: p1 p2
[ 1.580000] EXT3-fs: barriers not enabled
[ 6.770000] kjournald starting. Commit interval 5 seconds
[ 7.510000] EXT3-fs (mmcblk0p2): using internal journal
[ 7.510000] EXT3-fs (mmcblk0p2): recovery complete
[ 7.520000] EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
[ 7.530000] VFS: Mounted root (ext3 filesystem) on device 179:2.
[ 7.540000] devtmpfs: mounted
[ 7.540000] Freeing init memory: 172K
INIT: version 2.86 booting
Please wait: booting...
Error opening /dev/fb0: No such file or directory
Starting udev
WARNING: -e needs -E or -F
[ 8.190000] udevd (67): /proc/67/oom_adj is deprecated, please use /proc/67/oom_score_adj instead.
Remounting root file system...
Caching udev devnodes
Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory
ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1625: No soundcards found...
Configuring update-modules.
Configuring omap3-sgx-modules.
Configuring ti-cmem-module.
Configuring ti-syslink-module.
Configuring dbus.
Adding system startup for /etc/init.d/dbus-1.
Configuring kernel-module-tunnel4.
Configuring kernel-module-sit.
Configuring kernel-module-xfrm6-mode-beet.
Configuring kernel-module-xfrm6-mode-tunnel.
Configuring kernel-module-xfrm6-mode-transport.
Configuring kernel-module-scsi-wait-scan.
Configuring kernel-module-ssb.
Configuring kernel-module-vpss.
Configuring kernel-module-sii9022a.
Configuring kernel-module-ti81xxhdmi.
Configuring kernel-module-ti81xxfb.
Configuring kernel-module-ti81xxvo.
Configuring kernel-image-2.6.37.
Configuring network interfaces... [ 56.630000] davinci_mdio davinci_mdio.0: resetting idled controller
[ 56.640000] net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014)
udhcpc (v1.13.2) started
Sending discover...
[ 58.640000] PHY: 0:01 - Link is Up - 100/Full
Sending discover...
Sending select for 172.16.3.46...
Lease of 172.16.3.46 obtained, lease time 600
adding dns 172.16.1.10
done.
Setting up IP spoofing protection: rp_filter.
hwclock: can't open '/dev/misc/rtc': No such file or directory
Thu Sep 8 14:28:00 UTC 2011
hwclock: can't open '/dev/misc/rtc': No such file or directory
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Loading HDVICP2 Firmware
DM816X prcm_config_app version: 2.0.0.1
Doing PRCM settings...
PRCM for IVHD0 is in Progress, Please wait.....
BW Phy Addr : 0x48180600 Data : 0x00000002
AW Phy Addr : 0x48180600 Data : 0x00000002
Phy Addr : 0x48180c04 Data : 0x00000037
BW Phy Addr : 0x48180620 Data : 0x00070000
AW Phy Addr : 0x48180620 Data : 0x00070002
BW Phy Addr : 0x48180624 Data : 0x00030000
AW Phy Addr : 0x48180624 Data : 0x00010002
Phy Addr : 0x48180600 Data : 0x00000102
BW Phy Addr : 0x48180c10 Data : 0x00000007
AW Phy Addr : 0x48180c10 Data : 0x00000003
Phy Addr : 0x48180c14 Data : 0x00000004
BW Phy Addr : 0x58088000 Data : 0x447e1228
AW Phy Addr : 0x58088000 Data : 0xeafffffe
BW Phy Addr : 0x58098000 Data : 0x13fb9627
AW Phy Addr : 0x58098000 Data : 0xeafffffe
BW Phy Addr : 0x48180c10 Data : 0x00000003
AW Phy Addr : 0x48180c10 Data : 0x00000000
Phy Addr : 0x48180c14 Data : 0x00000007
PRCM for IVHD0 is Done Successfully
PRCM for IVHD1 is in Progress, Please wait.....
BW Phy Addr : 0x48180700 Data : 0x00000002
AW Phy Addr : 0x48180700 Data : 0x00000002
Phy Addr : 0x48180d04 Data : 0x00000037
BW Phy Addr : 0x48180720 Data : 0x00070000
AW Phy Addr : 0x48180720 Data : 0x00050002
BW Phy Addr : 0x48180724 Data : 0x00030000
AW Phy Addr : 0x48180724 Data : 0x00010002
Phy Addr : 0x48180700 Data : 0x00000102
BW Phy Addr : 0x48180d10 Data : 0x00000007
AW Phy Addr : 0x48180d10 Data : 0x00000003
Phy Addr : 0x48180d14 Data : 0x00000004
BW Phy Addr : 0x5a088000 Data : 0xe2cf6ed9
AW Phy Addr : 0x5a088000 Data : 0xeafffffe
BW Phy Addr : 0x5a098000 Data : 0xa2856ddd
AW Phy Addr : 0x5a098000 Data : 0xeafffffe
BW Phy Addr : 0x48180d10 Data : 0x00000003
AW Phy Addr : 0x48180d10 Data : 0x00000000
Phy Addr : 0x48180d14 Data : 0x00000007
PRCM for IVHD1 is Done Successfully
PRCM for IVHD2 is in Progress, Please wait.....
BW Phy Addr : 0x48180800 Data : 0x00000002
AW Phy Addr : 0x48180800 Data : 0x00000002
Phy Addr : 0x48180e04 Data : 0x00000037
BW Phy Addr : 0x48180820 Data : 0x00070000
AW Phy Addr : 0x48180820 Data : 0x00050002
BW Phy Addr : 0x48180824 Data : 0x00030000
AW Phy Addr : 0x48180824 Data : 0x00010002
Phy Addr : 0x48180800 Data : 0x00000102
BW Phy Addr : 0x48180e10 Data : 0x00000007
AW Phy Addr : 0x48180e10 Data : 0x00000003
Phy Addr : 0x48180e14 Data : 0x00000004
BW Phy Addr : 0x53088000 Data : 0x34fd6e45
AW Phy Addr : 0x53088000 Data : 0xeafffffe
BW Phy Addr : 0x53098000 Data : 0x708bda47
AW Phy Addr : 0x53098000 Data : 0xeafffffe
BW Phy Addr : 0x48180e10 Data : 0x00000003
AW Phy Addr : 0x48180e10 Data : 0x00000000
Phy Addr : 0x48180e14 Data : 0x00000007
PRCM for IVHD2 is Done Successfully
PRCM Initialization completed
[ 66.240000] SysLink version : 2.00.02.80
[ 66.240000] SysLink module created on Date:Sep 8 2011 Time:12:18:39
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.1.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 1 start Successful
Starting telnet daemon.
Loading HDVPSS Firmware
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.1.1
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 2 start Successful
cat: write error: No space left on device
cat: write error: No space left on device
[ 86.540000] HDMI W1 rev 2.0
Starting syslogd/klogd: done
Starting thttpd.
Starting PVR
/dev/mem opened.
Memory mapped at address 0x40282000.
Read at address 0x48180F04 (0x40282f04): 0x00000001
Write at address 0x48180F04 (0x40282f04): 0x00000000, readback 0x00000000
/dev/mem opened.
Memory mapped at address 0x401f3000.
Read at address 0x48180900 (0x401f3900): 0x00000102
Write at address 0x48180900 (0x401f3900): 0x00000002, readback 0x00000002
/dev/mem opened.
Memory mapped at address 0x401af000.
Read at address 0x48180920 (0x401af920): 0x00040002
Write at address 0x48180920 (0x401af920): 0x00000002, readback 0x00000002
/etc/init.d/rc: line 172: /etc/rc5.d/S90ipc6run: Permission denied

_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|

Arago Project http://arago-project.org dm816x-evm ttyO2

Arago 2011.05 dm816x-evm ttyO2

dm816x-evm login:

Regards,

Lei Wong