This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Enabling Camera application on Android ICS (4.0.3).

Dear All

Good Morning!

What i am doing:

i have followed the following links to enable the USB-Camera on "Android ICS 4.0.3" on  "Beagleboard-xm Rev C".

1) http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3.4-DevKit-2.1_PortingGuides#Camera

2) http://e2e.ti.com/support/embedded/android/f/509/p/158688/580245.aspx

I have followed  the same process which was suggested in the 2nd link. based on that i am sending the log file attached.

When i click the Camera application on "Launcher", i see the following message "Unfortunately, Camera has stopped."

i have take a log of this also which is in the same log file.

I have done all the changes required suggested in link 1 and 2.

What i want:

I want  to use the camera application and to  see the image on the screen, when the Usb camera is connected to the board.

Type of camera Logitech USB.

I have configured all the drivers of Logitech using " Driver Configuration  " and build the Kernel uImage.

I would be thankful for the guidence to make it work (Camera Application on connecting USB CAMERA).

5224.TICAMARALOG.txt

Regards

Aslam

  • Dear All

    Good Morning!

    I am sorry, that i didnt provide the logs of the following things:

    1) $cd  /sys/class/video4linux/videox

    2) $cat name

    Please look into this logs also where it has the outputs of the following commands  in "catname.rtf"

    Please guide us, so that the camera application works.

    0207.catname.rtf

    Regards

    Aslam

  • Hello!!

    I know it's been a while, but I'm working with the BeagleBoard-xm too, I want to activate an USB camera. Can you explain me how you did that?.

    I'm using Android 4.0.3 too, I can compile the kernel and I tried to activate some webcam drivers, but it still doesn't work.

    In some of your posts, I read that you gave some permisions to the video, how did you do that, please I' ve  been trying this for a long time with no sucess.

    Thanks for your answer.