hi,
I'm using TMDSEVMC6472,CCSv4.2,sys/bios6.3.mcsdk1.0
in the .cfg file ,we can config the sectMap ,like DDR2,LLRAM,SLRAM. then,in the project directory will generate a .map file,e.g.
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
SL2RAM 00200000 000c0000 00058530 00067ad0 RW X
LL2RAM 00800000 00098000 00000200 00097e00 RW X
DDR2 e0000000 10000000 000b0621 0ff4f9df RWIX
I know in my board,the DDR2 start addr is 0xe0000000 ,but i want to retain some space 0xe0000000~0xe1000000,and the project can use from 0xe1000000,not 0xe0000000,
how can i modify? thank you !
In fact ,I have changed the nimu,than the client example can run the core1 not only the core0,it succeed !
now I want to both running a client example on core0 and core1,so I think I must distinguish the space in the DDR2 and SLRAM for the two cores running clients.
maybe change like the follows:
SL2RAM 00260000 000c0000 00058530 00067ad0 RW X
LL2RAM 00800000 00098000 00000200 00097e00 RW X
DDR2 e1000000 10000000 000b0621 0ff4f9df RWIX