This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hyperlink question

Hi,

I would like to know the different configurations that can be done by using hyperlink, in terms of the type and the number of devices that can be connected together?

Thanks,

Miguel Aguilar

  • Miguel,

    The architecture of Hyperlink is simply a point-to-point communication.  So, you can only connect two devices together.  We currently support connection between two Keystone devices, and are working with a few FPGA manufacturers to allow connetion between an FPGA and a Keystone device.  In the future, it's possible that there will be two instances of hyperlink implemented on devices, allowing communication in a ring fashion.  But, all devices that exist today have only a single instance.

    Regards,
    Dan