Other Parts Discussed in Thread: AM3359
Hi all.
I want to change the cpu clock speed of AM3359 ICE demoboard. The default value is 550MHz, as defined in "ti.platforms.evmAM3359".
I followed this procedure:
- edit a new custom platform based on "ti.platforms.evmAM3359", with 720MHz clock instead of 550MHz.
- selected this new platofrm definition in RTSC options.
- cleaned and built the example project (uartecho demo as provided with the sdk) with no error; the console output reflected the new platform selection.
Unfortunately no changes automatically occurred in sys/bios config file (uart_echo.cfg). I didn't find out where select a different platform!
Downloading the binary results in a stop caused by 32768Hz timer mismatch.
Is it possibile to update the cpu clock frequency in an existing project, or I have to create a brand new project?