Other Parts Discussed in Thread: DM3725, DM3730
Hi,
we are working on a design using the DM3725/30.
Our choice of processor was driven by DSP performance requirements and cost targets.
We are now looking at OS selection, and I would like to hear experiences and opinions from other people.
Our application/system would naturally fit with a simple OS (e.g.: TI SYS/BIOS) with a couple of devices drivers (USB device, NAND Flash, eMMC, UART,SPI,I2C, DSPLink) and some middleware to it (file system on Flash, USB device stack, DSPLink).
The low effort route (at least to get started) is TI's DVSDK, as it has all the above already in place. But for us Linux is an overkill and a bit of a nuissance (e.g.: big boot time, big memory footprint). I understand that Linux on DVSDK is the only PSP/BSP supported by TI for this device, which is a shame, because we could do with TI SYS/BIOS; which I understand is support for this device but with none of our required middleware nor device drivers.
I have started to talk to all the embedded OS vendors mentioned on the DM3730 site, but would love to hear other people experiences, thoughts or suggestions.
Thanks,
Raul