Other Parts Discussed in Thread: AM3715, OMAP3530, DAC7512, TCA6416, TCA8418, LM8323, TPS65010, TPS65910, TPS65912, TWL6030, TWL6040, BQ24022, LP3971, LP3972, TPS65023, LM3530, LP3944, LP5521, LP5523, DAC124S085, TCA6507
Hi All,
I am working on a Beagleboard based platform using AM3715. The application and hardware I have is the following:
AM3715 -> TIUSB1210 (USBxceiver) -> CARL9170 (Atheros Radio)
I havent been able to detect to the USB connection to the ATH Radio.
From the logs I see the following:
[ 4.159027] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller!!!!
[ 4.165313] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
[ 4.173187] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
[ 4.193054] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 4.199218] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 4.206329] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.213867] usb usb1: Product: OMAP-EHCI Host Controller!!!!
[ 4.219787] usb usb1: Manufacturer: Linux 3.3.0 ehci_hcd
[ 4.225341] usb usb1: SerialNumber: ehci-omap.0
[ 4.231079] hub 1-0:1.0: USB hub found
[ 4.235107] hub 1-0:1.0: 3 ports detected
Moreover I have two GPIOS one is gpio_149 which is the USB_reset to the xceiver and gpio_129 which is the power to radio chip.
TIUSB1210 power is ok, clock is 60MHz and power to Radio is fine. I would expect to see an autodetection in the usb-hub side to mount the device right?
From board config I have this setup:
/* Muxing GPIOS */
static struct omap_board_mux board_mux[] __initdata =
{
OMAP3_MUX(UART1_RTS, OMAP_MUX_MODE4 | OMAP_PIN_OUTPUT), //149 Reset to radio USB
OMAP3_MUX(UART1_RX, OMAP_MUX_MODE4 | OMAP_PIN_OUTPUT), //151
{ .reg_offset = OMAP_MUX_TERMINATOR },
};
/* USB DATA */
static const struct usbhs_omap_board_data usbhs_bdata __initconst = {
.port_mode[0] = OMAP_EHCI_PORT_MODE_PHY,
.port_mode[1] = OMAP_USBHS_PORT_MODE_UNUSED,
.port_mode[2] = OMAP_USBHS_PORT_MODE_UNUSED,
.phy_reset = true,
.reset_gpio_port[0] = -EINVAL,
.reset_gpio_port[1] = -EINVAL,
.reset_gpio_port[2] = -EINVAL
};
If anybody knows what is wrong I would really appreciate it.
Regards,
My .config is the following:
#
# Automatically generated file; DO NOT EDIT.
# Linux/arm 3.3.0 Kernel Configuration
#
CONFIG_ARM=y
CONFIG_SYS_SUPPORTS_APM_EMULATION=y
CONFIG_HAVE_SCHED_CLOCK=y
CONFIG_GENERIC_GPIO=y
# CONFIG_ARCH_USES_GETTIMEOFFSET is not set
CONFIG_GENERIC_CLOCKEVENTS=y
CONFIG_KTIME_SCALAR=y
CONFIG_HAVE_PROC_CPU=y
CONFIG_STACKTRACE_SUPPORT=y
CONFIG_HAVE_LATENCYTOP_SUPPORT=y
CONFIG_LOCKDEP_SUPPORT=y
CONFIG_TRACE_IRQFLAGS_SUPPORT=y
CONFIG_HARDIRQS_SW_RESEND=y
CONFIG_GENERIC_IRQ_PROBE=y
CONFIG_RWSEM_GENERIC_SPINLOCK=y
CONFIG_ARCH_HAS_CPUFREQ=y
CONFIG_ARCH_HAS_CPU_IDLE_WAIT=y
CONFIG_GENERIC_HWEIGHT=y
CONFIG_GENERIC_CALIBRATE_DELAY=y
CONFIG_NEED_DMA_MAP_STATE=y
CONFIG_VECTORS_BASE=0xffff0000
# CONFIG_ARM_PATCH_PHYS_VIRT is not set
CONFIG_PHYS_OFFSET=0x80000000
CONFIG_GENERIC_BUG=y
CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"
CONFIG_HAVE_IRQ_WORK=y
CONFIG_IRQ_WORK=y
#
# General setup
#
CONFIG_EXPERIMENTAL=y
CONFIG_BROKEN_ON_SMP=y
CONFIG_INIT_ENV_ARG_LIMIT=32
CONFIG_CROSS_COMPILE=""
CONFIG_LOCALVERSION=""
# CONFIG_LOCALVERSION_AUTO is not set
CONFIG_HAVE_KERNEL_GZIP=y
CONFIG_HAVE_KERNEL_LZMA=y
CONFIG_HAVE_KERNEL_XZ=y
CONFIG_HAVE_KERNEL_LZO=y
# CONFIG_KERNEL_GZIP is not set
CONFIG_KERNEL_LZMA=y
# CONFIG_KERNEL_XZ is not set
# CONFIG_KERNEL_LZO is not set
CONFIG_DEFAULT_HOSTNAME="(none)"
CONFIG_SWAP=y
CONFIG_SYSVIPC=y
CONFIG_SYSVIPC_SYSCTL=y
CONFIG_POSIX_MQUEUE=y
CONFIG_POSIX_MQUEUE_SYSCTL=y
CONFIG_BSD_PROCESS_ACCT=y
# CONFIG_BSD_PROCESS_ACCT_V3 is not set
# CONFIG_FHANDLE is not set
# CONFIG_TASKSTATS is not set
# CONFIG_AUDIT is not set
CONFIG_HAVE_GENERIC_HARDIRQS=y
#
# IRQ subsystem
#
CONFIG_GENERIC_HARDIRQS=y
CONFIG_HAVE_SPARSE_IRQ=y
CONFIG_GENERIC_IRQ_SHOW=y
CONFIG_GENERIC_IRQ_CHIP=y
CONFIG_IRQ_DOMAIN=y
# CONFIG_SPARSE_IRQ is not set
#
# RCU Subsystem
#
CONFIG_TINY_PREEMPT_RCU=y
CONFIG_PREEMPT_RCU=y
# CONFIG_RCU_TRACE is not set
# CONFIG_TREE_RCU_TRACE is not set
# CONFIG_RCU_BOOST is not set
# CONFIG_IKCONFIG is not set
CONFIG_LOG_BUF_SHIFT=16
# CONFIG_CGROUPS is not set
# CONFIG_CHECKPOINT_RESTORE is not set
CONFIG_NAMESPACES=y
# CONFIG_UTS_NS is not set
# CONFIG_IPC_NS is not set
CONFIG_USER_NS=y
# CONFIG_PID_NS is not set
CONFIG_NET_NS=y
# CONFIG_SCHED_AUTOGROUP is not set
# CONFIG_SYSFS_DEPRECATED is not set
# CONFIG_RELAY is not set
CONFIG_BLK_DEV_INITRD=y
CONFIG_INITRAMFS_SOURCE="/home/fedex/openwrt/backfire/build_dir/target-arm_v5te_uClibc-0.9.33.2_eabi/root-omap35xx /home/fedex/openwrt/backfire/target/linux/generic/image/initramfs-base-files.txt"
CONFIG_INITRAMFS_ROOT_UID=1000
CONFIG_INITRAMFS_ROOT_GID=1000
# CONFIG_RD_GZIP is not set
# CONFIG_RD_BZIP2 is not set
CONFIG_RD_LZMA=y
# CONFIG_RD_XZ is not set
# CONFIG_RD_LZO is not set
# CONFIG_INITRAMFS_COMPRESSION_NONE is not set
CONFIG_INITRAMFS_COMPRESSION_LZMA=y
# CONFIG_CC_OPTIMIZE_FOR_SIZE is not set
CONFIG_SYSCTL=y
CONFIG_ANON_INODES=y
CONFIG_EXPERT=y
CONFIG_UID16=y
# CONFIG_SYSCTL_SYSCALL is not set
# CONFIG_KALLSYMS is not set
CONFIG_HOTPLUG=y
CONFIG_PRINTK=y
CONFIG_BUG=y
CONFIG_ELF_CORE=y
CONFIG_BASE_FULL=y
CONFIG_FUTEX=y
CONFIG_EPOLL=y
CONFIG_SIGNALFD=y
CONFIG_TIMERFD=y
CONFIG_EVENTFD=y
CONFIG_SHMEM=y
# CONFIG_AIO is not set
CONFIG_EMBEDDED=y
CONFIG_HAVE_PERF_EVENTS=y
CONFIG_PERF_USE_VMALLOC=y
#
# Kernel Performance Events And Counters
#
CONFIG_PERF_EVENTS=y
# CONFIG_PERF_COUNTERS is not set
# CONFIG_DEBUG_PERF_USE_VMALLOC is not set
# CONFIG_VM_EVENT_COUNTERS is not set
# CONFIG_COMPAT_BRK is not set
CONFIG_SLAB=y
# CONFIG_SLUB is not set
# CONFIG_SLOB is not set
# CONFIG_PROFILING is not set
CONFIG_HAVE_OPROFILE=y
# CONFIG_KPROBES is not set
CONFIG_HAVE_KPROBES=y
CONFIG_HAVE_KRETPROBES=y
CONFIG_HAVE_REGS_AND_STACK_ACCESS_API=y
CONFIG_HAVE_CLK=y
CONFIG_HAVE_DMA_API_DEBUG=y
CONFIG_HAVE_HW_BREAKPOINT=y
#
# GCOV-based kernel profiling
#
# CONFIG_GCOV_KERNEL is not set
CONFIG_HAVE_GENERIC_DMA_COHERENT=y
CONFIG_SLABINFO=y
CONFIG_RT_MUTEXES=y
CONFIG_BASE_SMALL=0
CONFIG_MODULES=y
# CONFIG_MODULE_FORCE_LOAD is not set
CONFIG_MODULE_UNLOAD=y
# CONFIG_MODULE_FORCE_UNLOAD is not set
# CONFIG_MODVERSIONS is not set
# CONFIG_MODULE_SRCVERSION_ALL is not set
CONFIG_BLOCK=y
CONFIG_LBDAF=y
# CONFIG_BLK_DEV_BSG is not set
# CONFIG_BLK_DEV_BSGLIB is not set
# CONFIG_BLK_DEV_INTEGRITY is not set
#
# Partition Types
#
CONFIG_PARTITION_ADVANCED=y
# CONFIG_ACORN_PARTITION is not set
# CONFIG_OSF_PARTITION is not set
# CONFIG_AMIGA_PARTITION is not set
# CONFIG_ATARI_PARTITION is not set
# CONFIG_MAC_PARTITION is not set
CONFIG_MSDOS_PARTITION=y
# CONFIG_BSD_DISKLABEL is not set
# CONFIG_MINIX_SUBPARTITION is not set
# CONFIG_SOLARIS_X86_PARTITION is not set
# CONFIG_UNIXWARE_DISKLABEL is not set
# CONFIG_LDM_PARTITION is not set
# CONFIG_SGI_PARTITION is not set
# CONFIG_ULTRIX_PARTITION is not set
# CONFIG_SUN_PARTITION is not set
# CONFIG_KARMA_PARTITION is not set
CONFIG_EFI_PARTITION=y
# CONFIG_SYSV68_PARTITION is not set
#
# IO Schedulers
#
CONFIG_IOSCHED_NOOP=y
CONFIG_IOSCHED_DEADLINE=y
# CONFIG_IOSCHED_CFQ is not set
CONFIG_DEFAULT_DEADLINE=y
# CONFIG_DEFAULT_NOOP is not set
CONFIG_DEFAULT_IOSCHED="deadline"
# CONFIG_INLINE_SPIN_TRYLOCK is not set
# CONFIG_INLINE_SPIN_TRYLOCK_BH is not set
# CONFIG_INLINE_SPIN_LOCK is not set
# CONFIG_INLINE_SPIN_LOCK_BH is not set
# CONFIG_INLINE_SPIN_LOCK_IRQ is not set
# CONFIG_INLINE_SPIN_LOCK_IRQSAVE is not set
# CONFIG_INLINE_SPIN_UNLOCK is not set
# CONFIG_INLINE_SPIN_UNLOCK_BH is not set
# CONFIG_INLINE_SPIN_UNLOCK_IRQ is not set
# CONFIG_INLINE_SPIN_UNLOCK_IRQRESTORE is not set
# CONFIG_INLINE_READ_TRYLOCK is not set
# CONFIG_INLINE_READ_LOCK is not set
# CONFIG_INLINE_READ_LOCK_BH is not set
# CONFIG_INLINE_READ_LOCK_IRQ is not set
# CONFIG_INLINE_READ_LOCK_IRQSAVE is not set
# CONFIG_INLINE_READ_UNLOCK is not set
# CONFIG_INLINE_READ_UNLOCK_BH is not set
# CONFIG_INLINE_READ_UNLOCK_IRQ is not set
# CONFIG_INLINE_READ_UNLOCK_IRQRESTORE is not set
# CONFIG_INLINE_WRITE_TRYLOCK is not set
# CONFIG_INLINE_WRITE_LOCK is not set
# CONFIG_INLINE_WRITE_LOCK_BH is not set
# CONFIG_INLINE_WRITE_LOCK_IRQ is not set
# CONFIG_INLINE_WRITE_LOCK_IRQSAVE is not set
# CONFIG_INLINE_WRITE_UNLOCK is not set
# CONFIG_INLINE_WRITE_UNLOCK_BH is not set
# CONFIG_INLINE_WRITE_UNLOCK_IRQ is not set
# CONFIG_INLINE_WRITE_UNLOCK_IRQRESTORE is not set
# CONFIG_MUTEX_SPIN_ON_OWNER is not set
CONFIG_FREEZER=y
#
# System Type
#
CONFIG_MMU=y
# CONFIG_ARCH_INTEGRATOR is not set
# CONFIG_ARCH_REALVIEW is not set
# CONFIG_ARCH_VERSATILE is not set
# CONFIG_ARCH_VEXPRESS is not set
# CONFIG_ARCH_AT91 is not set
# CONFIG_ARCH_BCMRING is not set
# CONFIG_ARCH_HIGHBANK is not set
# CONFIG_ARCH_CLPS711X is not set
# CONFIG_ARCH_CNS3XXX is not set
# CONFIG_ARCH_GEMINI is not set
# CONFIG_ARCH_PRIMA2 is not set
# CONFIG_ARCH_EBSA110 is not set
# CONFIG_ARCH_EP93XX is not set
# CONFIG_ARCH_FOOTBRIDGE is not set
# CONFIG_ARCH_MXC is not set
# CONFIG_ARCH_MXS is not set
# CONFIG_ARCH_NETX is not set
# CONFIG_ARCH_H720X is not set
# CONFIG_ARCH_IOP13XX is not set
# CONFIG_ARCH_IOP32X is not set
# CONFIG_ARCH_IOP33X is not set
# CONFIG_ARCH_IXP23XX is not set
# CONFIG_ARCH_IXP2000 is not set
# CONFIG_ARCH_IXP4XX is not set
# CONFIG_ARCH_DOVE is not set
# CONFIG_ARCH_KIRKWOOD is not set
# CONFIG_ARCH_LPC32XX is not set
# CONFIG_ARCH_MV78XX0 is not set
# CONFIG_ARCH_ORION5X is not set
# CONFIG_ARCH_MMP is not set
# CONFIG_ARCH_KS8695 is not set
# CONFIG_ARCH_W90X900 is not set
# CONFIG_ARCH_TEGRA is not set
# CONFIG_ARCH_PICOXCELL is not set
# CONFIG_ARCH_PNX4008 is not set
# CONFIG_ARCH_PXA is not set
# CONFIG_ARCH_MSM is not set
# CONFIG_ARCH_SHMOBILE is not set
# CONFIG_ARCH_RPC is not set
# CONFIG_ARCH_SA1100 is not set
# CONFIG_ARCH_S3C2410 is not set
# CONFIG_ARCH_S3C64XX is not set
# CONFIG_ARCH_S5P64X0 is not set
# CONFIG_ARCH_S5PC100 is not set
# CONFIG_ARCH_S5PV210 is not set
# CONFIG_ARCH_EXYNOS is not set
# CONFIG_ARCH_SHARK is not set
# CONFIG_ARCH_U300 is not set
# CONFIG_ARCH_U8500 is not set
# CONFIG_ARCH_NOMADIK is not set
# CONFIG_ARCH_DAVINCI is not set
CONFIG_ARCH_OMAP=y
# CONFIG_PLAT_SPEAR is not set
# CONFIG_ARCH_VT8500 is not set
# CONFIG_ARCH_ZYNQ is not set
# CONFIG_GPIO_PCA953X is not set
# CONFIG_KEYBOARD_GPIO_POLLED is not set
#
# TI OMAP Common Features
#
CONFIG_ARCH_OMAP_OTG=y
# CONFIG_ARCH_OMAP1 is not set
CONFIG_ARCH_OMAP2PLUS=y
#
# OMAP Feature Selections
#
# CONFIG_OMAP_SMARTREFLEX is not set
CONFIG_OMAP_RESET_CLOCKS=y
CONFIG_OMAP_MUX=y
CONFIG_OMAP_MUX_DEBUG=y
CONFIG_OMAP_MUX_WARNINGS=y
CONFIG_OMAP_MCBSP=y
# CONFIG_OMAP_MBOX_FWK is not set
CONFIG_OMAP_32K_TIMER=y
# CONFIG_OMAP3_L2_AUX_SECURE_SAVE_RESTORE is not set
CONFIG_OMAP_32K_TIMER_HZ=128
CONFIG_OMAP_DM_TIMER=y
CONFIG_OMAP_PM_NOOP=y
CONFIG_MACH_OMAP_GENERIC=y
#
# TI OMAP2/3/4 Specific Features
#
CONFIG_ARCH_OMAP2PLUS_TYPICAL=y
# CONFIG_ARCH_OMAP2 is not set
CONFIG_ARCH_OMAP3=y
# CONFIG_ARCH_OMAP4 is not set
CONFIG_SOC_OMAP3430=y
# CONFIG_SOC_OMAPTI81XX is not set
# CONFIG_SOC_OMAPAM33XX is not set
CONFIG_OMAP_PACKAGE_CBB=y
#
# OMAP Board Type
#
CONFIG_MACH_OMAP3_BEAGLE=y
# CONFIG_MACH_DEVKIT8000 is not set
# CONFIG_MACH_OMAP_LDP is not set
# CONFIG_MACH_OMAP3530_LV_SOM is not set
# CONFIG_MACH_OMAP3_TORPEDO is not set
# CONFIG_MACH_OVERO is not set
# CONFIG_MACH_OMAP3EVM is not set
# CONFIG_MACH_OMAP3517EVM is not set
# CONFIG_MACH_CRANEBOARD is not set
# CONFIG_MACH_OMAP3_PANDORA is not set
# CONFIG_MACH_OMAP3_TOUCHBOOK is not set
# CONFIG_MACH_OMAP_3430SDP is not set
# CONFIG_MACH_NOKIA_RM680 is not set
# CONFIG_MACH_NOKIA_RX51 is not set
# CONFIG_MACH_OMAP_ZOOM2 is not set
# CONFIG_MACH_OMAP_ZOOM3 is not set
# CONFIG_MACH_CM_T35 is not set
# CONFIG_MACH_CM_T3517 is not set
# CONFIG_MACH_IGEP0020 is not set
# CONFIG_MACH_IGEP0030 is not set
# CONFIG_MACH_SBC3530 is not set
# CONFIG_MACH_OMAP_3630SDP is not set
# CONFIG_OMAP3_EMU is not set
# CONFIG_OMAP3_SDRC_AC_TIMING is not set
#
# System MMU
#
#
# Processor Type
#
CONFIG_CPU_V7=y
CONFIG_CPU_32v6K=y
CONFIG_CPU_32v7=y
CONFIG_CPU_ABRT_EV7=y
CONFIG_CPU_PABRT_V7=y
CONFIG_CPU_CACHE_V7=y
CONFIG_CPU_CACHE_VIPT=y
CONFIG_CPU_COPY_V6=y
CONFIG_CPU_TLB_V7=y
CONFIG_CPU_HAS_ASID=y
CONFIG_CPU_CP15=y
CONFIG_CPU_CP15_MMU=y
#
# Processor Features
#
# CONFIG_ARM_LPAE is not set
# CONFIG_ARCH_PHYS_ADDR_T_64BIT is not set
CONFIG_ARM_THUMB=y
# CONFIG_ARM_THUMBEE is not set
# CONFIG_SWP_EMULATE is not set
# CONFIG_CPU_ICACHE_DISABLE is not set
# CONFIG_CPU_DCACHE_DISABLE is not set
# CONFIG_CPU_BPREDICT_DISABLE is not set
# CONFIG_CACHE_L2X0 is not set
CONFIG_ARM_L1_CACHE_SHIFT_6=y
CONFIG_ARM_L1_CACHE_SHIFT=6
CONFIG_ARM_DMA_MEM_BUFFERABLE=y
CONFIG_ARM_NR_BANKS=8
CONFIG_MULTI_IRQ_HANDLER=y
# CONFIG_ARM_ERRATA_430973 is not set
# CONFIG_ARM_ERRATA_458693 is not set
# CONFIG_ARM_ERRATA_460075 is not set
# CONFIG_ARM_ERRATA_720789 is not set
# CONFIG_ARM_ERRATA_743622 is not set
# CONFIG_ARM_ERRATA_751472 is not set
# CONFIG_ARM_ERRATA_754322 is not set
#
# Bus support
#
# CONFIG_PCI_SYSCALL is not set
# CONFIG_ARCH_SUPPORTS_MSI is not set
# CONFIG_PCCARD is not set
#
# Kernel Features
#
CONFIG_TICK_ONESHOT=y
CONFIG_NO_HZ=y
CONFIG_HIGH_RES_TIMERS=y
CONFIG_GENERIC_CLOCKEVENTS_BUILD=y
CONFIG_VMSPLIT_3G=y
# CONFIG_VMSPLIT_2G is not set
# CONFIG_VMSPLIT_1G is not set
CONFIG_PAGE_OFFSET=0xC0000000
CONFIG_ARCH_NR_GPIO=0
# CONFIG_PREEMPT_NONE is not set
# CONFIG_PREEMPT_VOLUNTARY is not set
CONFIG_PREEMPT=y
CONFIG_PREEMPT_COUNT=y
CONFIG_HZ=128
# CONFIG_THUMB2_KERNEL is not set
CONFIG_AEABI=y
# CONFIG_OABI_COMPAT is not set
CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y
# CONFIG_ARCH_SPARSEMEM_DEFAULT is not set
# CONFIG_ARCH_SELECT_MEMORY_MODEL is not set
CONFIG_HAVE_ARCH_PFN_VALID=y
CONFIG_HIGHMEM=y
# CONFIG_HIGHPTE is not set
CONFIG_SELECT_MEMORY_MODEL=y
CONFIG_FLATMEM_MANUAL=y
CONFIG_FLATMEM=y
CONFIG_FLAT_NODE_MEM_MAP=y
CONFIG_HAVE_MEMBLOCK=y
CONFIG_PAGEFLAGS_EXTENDED=y
CONFIG_SPLIT_PTLOCK_CPUS=4
# CONFIG_COMPACTION is not set
# CONFIG_PHYS_ADDR_T_64BIT is not set
CONFIG_ZONE_DMA_FLAG=0
CONFIG_BOUNCE=y
CONFIG_VIRT_TO_BUS=y
# CONFIG_KSM is not set
CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
CONFIG_NEED_PER_CPU_KM=y
# CONFIG_CLEANCACHE is not set
CONFIG_FORCE_MAX_ZONEORDER=11
CONFIG_LEDS=y
CONFIG_ALIGNMENT_TRAP=y
# CONFIG_UACCESS_WITH_MEMCPY is not set
# CONFIG_SECCOMP is not set
# CONFIG_CC_STACKPROTECTOR is not set
# CONFIG_DEPRECATED_PARAM_STRUCT is not set
#
# Boot options
#
CONFIG_USE_OF=y
CONFIG_ZBOOT_ROM_TEXT=0x0
CONFIG_ZBOOT_ROM_BSS=0x0
# CONFIG_ARM_APPENDED_DTB is not set
CONFIG_CMDLINE="root=/dev/mmcblk0p2 rootwait console=ttyO2,115200"
CONFIG_CMDLINE_FROM_BOOTLOADER=y
# CONFIG_CMDLINE_EXTEND is not set
# CONFIG_CMDLINE_FORCE is not set
# CONFIG_XIP_KERNEL is not set
CONFIG_KEXEC=y
CONFIG_ATAGS_PROC=y
# CONFIG_CRASH_DUMP is not set
CONFIG_AUTO_ZRELADDR=y
#
# CPU Power Management
#
#
# CPU Frequency scaling
#
# CONFIG_CPU_FREQ is not set
CONFIG_CPU_IDLE=y
CONFIG_CPU_IDLE_GOV_LADDER=y
CONFIG_CPU_IDLE_GOV_MENU=y
#
# Floating point emulation
#
#
# At least one emulation must be selected
#
CONFIG_VFP=y
CONFIG_VFPv3=y
CONFIG_NEON=y
#
# Userspace binary formats
#
CONFIG_BINFMT_ELF=y
CONFIG_ARCH_BINFMT_ELF_RANDOMIZE_PIE=y
# CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS is not set
CONFIG_HAVE_AOUT=y
# CONFIG_BINFMT_AOUT is not set
CONFIG_BINFMT_MISC=y
#
# Power management options
#
CONFIG_SUSPEND=y
CONFIG_SUSPEND_FREEZER=y
CONFIG_PM_SLEEP=y
CONFIG_PM_RUNTIME=y
CONFIG_PM=y
CONFIG_PM_DEBUG=y
# CONFIG_PM_ADVANCED_DEBUG is not set
# CONFIG_PM_TEST_SUSPEND is not set
CONFIG_CAN_PM_TRACE=y
# CONFIG_APM_EMULATION is not set
CONFIG_ARCH_HAS_OPP=y
CONFIG_PM_OPP=y
CONFIG_PM_CLK=y
CONFIG_CPU_PM=y
CONFIG_ARCH_SUSPEND_POSSIBLE=y
CONFIG_ARM_CPU_SUSPEND=y
CONFIG_NET=y
#
# Networking options
#
CONFIG_PACKET=y
CONFIG_UNIX=y
# CONFIG_UNIX_DIAG is not set
# CONFIG_NET_KEY is not set
CONFIG_INET=y
CONFIG_IP_MULTICAST=y
CONFIG_IP_ADVANCED_ROUTER=y
# CONFIG_IP_FIB_TRIE_STATS is not set
CONFIG_IP_MULTIPLE_TABLES=y
CONFIG_IP_ROUTE_MULTIPATH=y
CONFIG_IP_ROUTE_VERBOSE=y
# CONFIG_IP_PNP is not set
# CONFIG_NET_IPIP is not set
# CONFIG_NET_IPGRE_DEMUX is not set
CONFIG_IP_MROUTE=y
CONFIG_IP_MROUTE_MULTIPLE_TABLES=y
# CONFIG_IP_PIMSM_V1 is not set
# CONFIG_IP_PIMSM_V2 is not set
CONFIG_ARPD=y
CONFIG_SYN_COOKIES=y
# CONFIG_INET_AH is not set
# CONFIG_INET_ESP is not set
# CONFIG_INET_IPCOMP is not set
# CONFIG_INET_XFRM_TUNNEL is not set
# CONFIG_INET_TUNNEL is not set
# CONFIG_INET_XFRM_MODE_TRANSPORT is not set
# CONFIG_INET_XFRM_MODE_TUNNEL is not set
# CONFIG_INET_XFRM_MODE_BEET is not set
# CONFIG_INET_LRO is not set
# CONFIG_INET_DIAG is not set
CONFIG_TCP_CONG_ADVANCED=y
# CONFIG_TCP_CONG_BIC is not set
# CONFIG_TCP_CONG_CUBIC is not set
CONFIG_TCP_CONG_WESTWOOD=y
# CONFIG_TCP_CONG_HTCP is not set
# CONFIG_TCP_CONG_HSTCP is not set
# CONFIG_TCP_CONG_HYBLA is not set
# CONFIG_TCP_CONG_VEGAS is not set
# CONFIG_TCP_CONG_SCALABLE is not set
# CONFIG_TCP_CONG_LP is not set
# CONFIG_TCP_CONG_VENO is not set
# CONFIG_TCP_CONG_YEAH is not set
# CONFIG_TCP_CONG_ILLINOIS is not set
CONFIG_DEFAULT_WESTWOOD=y
# CONFIG_DEFAULT_RENO is not set
CONFIG_DEFAULT_TCP_CONG="westwood"
# CONFIG_TCP_MD5SIG is not set
# CONFIG_IPV6 is not set
# CONFIG_NETWORK_SECMARK is not set
# CONFIG_NETWORK_PHY_TIMESTAMPING is not set
# CONFIG_NETFILTER is not set
# CONFIG_IP_DCCP is not set
# CONFIG_IP_SCTP is not set
# CONFIG_RDS is not set
# CONFIG_TIPC is not set
# CONFIG_ATM is not set
# CONFIG_L2TP is not set
CONFIG_STP=y
CONFIG_BRIDGE=y
# CONFIG_BRIDGE_IGMP_SNOOPING is not set
# CONFIG_NET_DSA is not set
CONFIG_VLAN_8021Q=y
# CONFIG_VLAN_8021Q_GVRP is not set
# CONFIG_DECNET is not set
CONFIG_LLC=y
# CONFIG_LLC2 is not set
# CONFIG_IPX is not set
# CONFIG_ATALK is not set
# CONFIG_X25 is not set
# CONFIG_LAPB is not set
# CONFIG_ECONET is not set
# CONFIG_WAN_ROUTER is not set
# CONFIG_PHONET is not set
# CONFIG_IEEE802154 is not set
CONFIG_NET_SCHED=y
#
# Queueing/Scheduling
#
# CONFIG_NET_SCH_CBQ is not set
# CONFIG_NET_SCH_HTB is not set
# CONFIG_NET_SCH_HFSC is not set
# CONFIG_NET_SCH_PRIO is not set
# CONFIG_NET_SCH_MULTIQ is not set
# CONFIG_NET_SCH_RED is not set
# CONFIG_NET_SCH_SFB is not set
# CONFIG_NET_SCH_SFQ is not set
# CONFIG_NET_SCH_ESFQ is not set
# CONFIG_NET_SCH_TEQL is not set
# CONFIG_NET_SCH_TBF is not set
# CONFIG_NET_SCH_GRED is not set
# CONFIG_NET_SCH_DSMARK is not set
# CONFIG_NET_SCH_NETEM is not set
# CONFIG_NET_SCH_DRR is not set
# CONFIG_NET_SCH_MQPRIO is not set
# CONFIG_NET_SCH_CHOKE is not set
# CONFIG_NET_SCH_QFQ is not set
#
# Classification
#
# CONFIG_NET_CLS_BASIC is not set
# CONFIG_NET_CLS_TCINDEX is not set
# CONFIG_NET_CLS_ROUTE4 is not set
# CONFIG_NET_CLS_FW is not set
# CONFIG_NET_CLS_U32 is not set
# CONFIG_NET_CLS_RSVP is not set
# CONFIG_NET_CLS_RSVP6 is not set
# CONFIG_NET_CLS_FLOW is not set
# CONFIG_NET_EMATCH is not set
# CONFIG_NET_CLS_ACT is not set
CONFIG_NET_SCH_FIFO=y
# CONFIG_DCB is not set
# CONFIG_BATMAN_ADV is not set
# CONFIG_OPENVSWITCH is not set
CONFIG_BQL=y
#
# Network testing
#
# CONFIG_NET_PKTGEN is not set
CONFIG_HAMRADIO=y
#
# Packet Radio protocols
#
# CONFIG_AX25 is not set
# CONFIG_CAN is not set
# CONFIG_IRDA is not set
# CONFIG_BT is not set
# CONFIG_AF_RXRPC is not set
CONFIG_FIB_RULES=y
CONFIG_WIRELESS=y
CONFIG_WIRELESS_EXT=y
CONFIG_WEXT_CORE=y
CONFIG_WEXT_PROC=y
CONFIG_WEXT_SPY=y
CONFIG_WEXT_PRIV=y
# CONFIG_CFG80211 is not set
# CONFIG_WIRELESS_EXT_SYSFS is not set
# CONFIG_LIB80211 is not set
# CONFIG_LIB80211_CRYPT_WEP is not set
# CONFIG_LIB80211_CRYPT_CCMP is not set
# CONFIG_LIB80211_CRYPT_TKIP is not set
#
# CFG80211 needs to be enabled for MAC80211
#
# CONFIG_WIMAX is not set
# CONFIG_RFKILL is not set
# CONFIG_RFKILL_REGULATOR is not set
# CONFIG_NET_9P is not set
# CONFIG_CAIF is not set
# CONFIG_CEPH_LIB is not set
# CONFIG_NFC is not set
#
# Device Drivers
#
#
# Generic Driver Options
#
CONFIG_UEVENT_HELPER_PATH="/sbin/hotplug"
# CONFIG_DEVTMPFS is not set
CONFIG_STANDALONE=y
CONFIG_PREVENT_FIRMWARE_BUILD=y
CONFIG_FW_LOADER=y
# CONFIG_FIRMWARE_IN_KERNEL is not set
CONFIG_EXTRA_FIRMWARE=""
# CONFIG_DEBUG_DRIVER is not set
# CONFIG_DEBUG_DEVRES is not set
# CONFIG_SYS_HYPERVISOR is not set
# CONFIG_GENERIC_CPU_DEVICES is not set
# CONFIG_DMA_SHARED_BUFFER is not set
# CONFIG_CONNECTOR is not set
CONFIG_MTD=y
# CONFIG_MTD_TESTS is not set
# CONFIG_MTD_ROOTFS_ROOT_DEV is not set
# CONFIG_MTD_ROOTFS_SPLIT is not set
# CONFIG_MTD_REDBOOT_PARTS is not set
CONFIG_MTD_CMDLINE_PARTS=y
# CONFIG_MTD_AFS_PARTS is not set
# CONFIG_MTD_OF_PARTS is not set
# CONFIG_MTD_AR7_PARTS is not set
#
# User Modules And Translation Layers
#
CONFIG_MTD_CHAR=y
CONFIG_MTD_BLKDEVS=y
CONFIG_MTD_BLOCK=y
# CONFIG_FTL is not set
# CONFIG_NFTL is not set
# CONFIG_INFTL is not set
# CONFIG_RFD_FTL is not set
# CONFIG_SSFDC is not set
# CONFIG_SM_FTL is not set
# CONFIG_MTD_OOPS is not set
# CONFIG_MTD_SWAP is not set
#
# RAM/ROM/Flash chip drivers
#
CONFIG_MTD_CFI=y
# CONFIG_MTD_JEDECPROBE is not set
CONFIG_MTD_GEN_PROBE=y
# CONFIG_MTD_CFI_ADV_OPTIONS is not set
CONFIG_MTD_MAP_BANK_WIDTH_1=y
CONFIG_MTD_MAP_BANK_WIDTH_2=y
CONFIG_MTD_MAP_BANK_WIDTH_4=y
# CONFIG_MTD_MAP_BANK_WIDTH_8 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_16 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_32 is not set
CONFIG_MTD_CFI_I1=y
CONFIG_MTD_CFI_I2=y
# CONFIG_MTD_CFI_I4 is not set
# CONFIG_MTD_CFI_I8 is not set
CONFIG_MTD_CFI_INTELEXT=y
CONFIG_MTD_CFI_AMDSTD=y
# CONFIG_MTD_CFI_STAA is not set
CONFIG_MTD_CFI_UTIL=y
# CONFIG_MTD_RAM is not set
# CONFIG_MTD_ROM is not set
# CONFIG_MTD_ABSENT is not set
#
# Mapping drivers for chip access
#
CONFIG_MTD_COMPLEX_MAPPINGS=y
# CONFIG_MTD_PHYSMAP is not set
# CONFIG_MTD_PHYSMAP_OF is not set
# CONFIG_MTD_GPIO_ADDR is not set
# CONFIG_MTD_PLATRAM is not set
# CONFIG_MTD_LATCH_ADDR is not set
#
# Self-contained MTD device drivers
#
# CONFIG_MTD_DATAFLASH is not set
# CONFIG_MTD_M25P80 is not set
# CONFIG_MTD_SST25L is not set
# CONFIG_MTD_SLRAM is not set
# CONFIG_MTD_PHRAM is not set
# CONFIG_MTD_MTDRAM is not set
# CONFIG_MTD_BLOCK2MTD is not set
#
# Disk-On-Chip Device Drivers
#
# CONFIG_MTD_DOC2000 is not set
# CONFIG_MTD_DOC2001 is not set
# CONFIG_MTD_DOC2001PLUS is not set
# CONFIG_MTD_DOCG3 is not set
CONFIG_MTD_NAND_ECC=y
# CONFIG_MTD_NAND_ECC_SMC is not set
CONFIG_MTD_NAND=y
CONFIG_MTD_NAND_VERIFY_WRITE=y
# CONFIG_MTD_NAND_ECC_BCH is not set
# CONFIG_MTD_SM_COMMON is not set
# CONFIG_MTD_NAND_MUSEUM_IDS is not set
# CONFIG_MTD_NAND_GPIO is not set
CONFIG_MTD_NAND_OMAP2=y
CONFIG_MTD_NAND_IDS=y
# CONFIG_MTD_NAND_DISKONCHIP is not set
# CONFIG_MTD_NAND_NANDSIM is not set
# CONFIG_MTD_NAND_PLATFORM is not set
# CONFIG_MTD_ALAUDA is not set
CONFIG_MTD_ONENAND=y
# CONFIG_MTD_ONENAND_VERIFY_WRITE is not set
# CONFIG_MTD_ONENAND_GENERIC is not set
# CONFIG_MTD_ONENAND_OMAP2 is not set
# CONFIG_MTD_ONENAND_OTP is not set
# CONFIG_MTD_ONENAND_2X_PROGRAM is not set
# CONFIG_MTD_ONENAND_SIM is not set
#
# LPDDR flash memory drivers
#
# CONFIG_MTD_LPDDR is not set
# CONFIG_MTD_UBI is not set
CONFIG_DTC=y
CONFIG_OF=y
#
# Device Tree and Open Firmware support
#
# CONFIG_PROC_DEVICETREE is not set
# CONFIG_OF_SELFTEST is not set
CONFIG_OF_FLATTREE=y
CONFIG_OF_EARLY_FLATTREE=y
CONFIG_OF_ADDRESS=y
CONFIG_OF_IRQ=y
CONFIG_OF_DEVICE=y
CONFIG_OF_GPIO=y
CONFIG_OF_I2C=y
CONFIG_OF_NET=y
CONFIG_OF_SPI=y
# CONFIG_PARPORT is not set
CONFIG_BLK_DEV=y
# CONFIG_BLK_DEV_COW_COMMON is not set
CONFIG_BLK_DEV_LOOP=y
CONFIG_BLK_DEV_LOOP_MIN_COUNT=8
# CONFIG_BLK_DEV_CRYPTOLOOP is not set
#
# DRBD disabled because PROC_FS, INET or CONNECTOR not selected
#
# CONFIG_BLK_DEV_NBD is not set
# CONFIG_BLK_DEV_UB is not set
CONFIG_BLK_DEV_RAM=y
CONFIG_BLK_DEV_RAM_COUNT=16
CONFIG_BLK_DEV_RAM_SIZE=16384
# CONFIG_BLK_DEV_XIP is not set
# CONFIG_CDROM_PKTCDVD is not set
# CONFIG_ATA_OVER_ETH is not set
# CONFIG_MG_DISK is not set
# CONFIG_BLK_DEV_RBD is not set
#
# Misc devices
#
# CONFIG_SENSORS_LIS3LV02D is not set
# CONFIG_AD525X_DPOT is not set
# CONFIG_ATMEL_PWM is not set
# CONFIG_ICS932S401 is not set
# CONFIG_ENCLOSURE_SERVICES is not set
# CONFIG_APDS9802ALS is not set
# CONFIG_ISL29003 is not set
# CONFIG_ISL29020 is not set
# CONFIG_SENSORS_TSL2550 is not set
# CONFIG_SENSORS_BH1780 is not set
# CONFIG_SENSORS_BH1770 is not set
# CONFIG_SENSORS_APDS990X is not set
# CONFIG_HMC6352 is not set
# CONFIG_DS1682 is not set
# CONFIG_TI_DAC7512 is not set
# CONFIG_BMP085 is not set
# CONFIG_USB_SWITCH_FSA9480 is not set
# CONFIG_C2PORT is not set
#
# EEPROM support
#
# CONFIG_EEPROM_AT24 is not set
# CONFIG_EEPROM_AT25 is not set
# CONFIG_EEPROM_LEGACY is not set
# CONFIG_EEPROM_MAX6875 is not set
# CONFIG_EEPROM_93CX6 is not set
# CONFIG_EEPROM_93XX46 is not set
# CONFIG_IWMC3200TOP is not set
#
# Texas Instruments shared transport line discipline
#
# CONFIG_TI_ST is not set
# CONFIG_SENSORS_LIS3_SPI is not set
# CONFIG_SENSORS_LIS3_I2C is not set
#
# Altera FPGA firmware download module
#
# CONFIG_ALTERA_STAPL is not set
#
# SCSI device support
#
CONFIG_SCSI_MOD=m
# CONFIG_RAID_ATTRS is not set
CONFIG_SCSI=m
CONFIG_SCSI_DMA=y
# CONFIG_SCSI_TGT is not set
# CONFIG_SCSI_NETLINK is not set
CONFIG_SCSI_PROC_FS=y
#
# SCSI support type (disk, tape, CD-ROM)
#
CONFIG_BLK_DEV_SD=m
# CONFIG_CHR_DEV_ST is not set
# CONFIG_CHR_DEV_OSST is not set
# CONFIG_BLK_DEV_SR is not set
# CONFIG_CHR_DEV_SG is not set
# CONFIG_CHR_DEV_SCH is not set
CONFIG_SCSI_MULTI_LUN=y
# CONFIG_SCSI_CONSTANTS is not set
# CONFIG_SCSI_LOGGING is not set
# CONFIG_SCSI_SCAN_ASYNC is not set
CONFIG_SCSI_WAIT_SCAN=m
#
# SCSI Transports
#
# CONFIG_SCSI_SPI_ATTRS is not set
# CONFIG_SCSI_FC_ATTRS is not set
# CONFIG_SCSI_ISCSI_ATTRS is not set
# CONFIG_SCSI_SAS_ATTRS is not set
# CONFIG_SCSI_SAS_LIBSAS is not set
# CONFIG_SCSI_SRP_ATTRS is not set
CONFIG_SCSI_LOWLEVEL=y
# CONFIG_ISCSI_TCP is not set
# CONFIG_ISCSI_BOOT_SYSFS is not set
# CONFIG_LIBFC is not set
# CONFIG_LIBFCOE is not set
# CONFIG_SCSI_DEBUG is not set
# CONFIG_SCSI_DH is not set
# CONFIG_SCSI_OSD_INITIATOR is not set
# CONFIG_ATA is not set
# CONFIG_MD is not set
# CONFIG_TARGET_CORE is not set
CONFIG_NETDEVICES=y
CONFIG_NET_CORE=y
# CONFIG_BONDING is not set
# CONFIG_DUMMY is not set
# CONFIG_EQUALIZER is not set
CONFIG_MII=y
# CONFIG_NET_TEAM is not set
# CONFIG_MACVLAN is not set
# CONFIG_NETCONSOLE is not set
# CONFIG_NETPOLL is not set
# CONFIG_NET_POLL_CONTROLLER is not set
# CONFIG_TUN is not set
# CONFIG_VETH is not set
#
# CAIF transport drivers
#
# CONFIG_ETHERNET is not set
# CONFIG_PHYLIB is not set
# CONFIG_MICREL_KS8995MA is not set
# CONFIG_PPP is not set
# CONFIG_SLIP is not set
#
# USB Network Adapters
#
# CONFIG_USB_CATC is not set
# CONFIG_USB_KAWETH is not set
# CONFIG_USB_PEGASUS is not set
# CONFIG_USB_RTL8150 is not set
CONFIG_USB_USBNET=y
# CONFIG_USB_NET_AX8817X is not set
# CONFIG_USB_NET_CDCETHER is not set
# CONFIG_USB_NET_CDC_EEM is not set
# CONFIG_USB_NET_CDC_NCM is not set
# CONFIG_USB_NET_DM9601 is not set
# CONFIG_USB_NET_SMSC75XX is not set
# CONFIG_USB_NET_SMSC95XX is not set
# CONFIG_USB_NET_GL620A is not set
# CONFIG_USB_NET_NET1080 is not set
# CONFIG_USB_NET_PLUSB is not set
# CONFIG_USB_NET_MCS7830 is not set
# CONFIG_USB_NET_RNDIS_HOST is not set
# CONFIG_USB_NET_CDC_SUBSET is not set
# CONFIG_USB_NET_ZAURUS is not set
# CONFIG_USB_NET_CX82310_ETH is not set
# CONFIG_USB_NET_KALMIA is not set
# CONFIG_USB_NET_INT51X1 is not set
# CONFIG_USB_IPHETH is not set
# CONFIG_USB_SIERRA_NET is not set
CONFIG_WLAN=y
# CONFIG_USB_ZD1201 is not set
# CONFIG_HOSTAP is not set
#
# Enable WiMAX (Networking options) to see the WiMAX drivers
#
# CONFIG_WAN is not set
# CONFIG_ISDN is not set
# CONFIG_PHONE is not set
#
# Input device support
#
CONFIG_INPUT=y
# CONFIG_INPUT_FF_MEMLESS is not set
# CONFIG_INPUT_POLLDEV is not set
# CONFIG_INPUT_SPARSEKMAP is not set
#
# Userland interfaces
#
# CONFIG_INPUT_MOUSEDEV is not set
CONFIG_INPUT_JOYDEV=y
CONFIG_INPUT_EVDEV=y
# CONFIG_INPUT_EVBUG is not set
#
# Input Device Drivers
#
CONFIG_INPUT_KEYBOARD=y
# CONFIG_KEYBOARD_ADP5588 is not set
# CONFIG_KEYBOARD_ADP5589 is not set
# CONFIG_KEYBOARD_ATKBD is not set
# CONFIG_KEYBOARD_QT1070 is not set
# CONFIG_KEYBOARD_QT2160 is not set
# CONFIG_KEYBOARD_LKKBD is not set
CONFIG_KEYBOARD_GPIO=y
# CONFIG_KEYBOARD_TCA6416 is not set
# CONFIG_KEYBOARD_TCA8418 is not set
# CONFIG_KEYBOARD_MATRIX is not set
# CONFIG_KEYBOARD_LM8323 is not set
# CONFIG_KEYBOARD_MAX7359 is not set
# CONFIG_KEYBOARD_MCS is not set
# CONFIG_KEYBOARD_MPR121 is not set
# CONFIG_KEYBOARD_NEWTON is not set
# CONFIG_KEYBOARD_OPENCORES is not set
# CONFIG_KEYBOARD_SAMSUNG is not set
# CONFIG_KEYBOARD_STOWAWAY is not set
# CONFIG_KEYBOARD_SUNKBD is not set
# CONFIG_KEYBOARD_TWL4030 is not set
# CONFIG_KEYBOARD_XTKBD is not set
# CONFIG_INPUT_MOUSE is not set
CONFIG_INPUT_JOYSTICK=y
# CONFIG_JOYSTICK_ANALOG is not set
# CONFIG_JOYSTICK_A3D is not set
# CONFIG_JOYSTICK_ADI is not set
# CONFIG_JOYSTICK_COBRA is not set
# CONFIG_JOYSTICK_GF2K is not set
# CONFIG_JOYSTICK_GRIP is not set
# CONFIG_JOYSTICK_GRIP_MP is not set
# CONFIG_JOYSTICK_GUILLEMOT is not set
# CONFIG_JOYSTICK_INTERACT is not set
# CONFIG_JOYSTICK_SIDEWINDER is not set
# CONFIG_JOYSTICK_TMDC is not set
# CONFIG_JOYSTICK_IFORCE is not set
# CONFIG_JOYSTICK_WARRIOR is not set
# CONFIG_JOYSTICK_MAGELLAN is not set
# CONFIG_JOYSTICK_SPACEORB is not set
# CONFIG_JOYSTICK_SPACEBALL is not set
# CONFIG_JOYSTICK_STINGER is not set
# CONFIG_JOYSTICK_TWIDJOY is not set
# CONFIG_JOYSTICK_ZHENHUA is not set
# CONFIG_JOYSTICK_AS5011 is not set
# CONFIG_JOYSTICK_JOYDUMP is not set
# CONFIG_JOYSTICK_XPAD is not set
# CONFIG_INPUT_TABLET is not set
# CONFIG_INPUT_TOUCHSCREEN is not set
# CONFIG_INPUT_MISC is not set
#
# Hardware I/O ports
#
# CONFIG_SERIO is not set
# CONFIG_GAMEPORT is not set
#
# Character devices
#
# CONFIG_VT is not set
CONFIG_UNIX98_PTYS=y
# CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set
# CONFIG_LEGACY_PTYS is not set
# CONFIG_SERIAL_NONSTANDARD is not set
# CONFIG_N_GSM is not set
# CONFIG_TRACE_SINK is not set
# CONFIG_DEVKMEM is not set
#
# Serial drivers
#
CONFIG_SERIAL_8250=y
CONFIG_SERIAL_8250_CONSOLE=y
CONFIG_SERIAL_8250_NR_UARTS=2
CONFIG_SERIAL_8250_RUNTIME_UARTS=2
# CONFIG_SERIAL_8250_EXTENDED is not set
# CONFIG_SERIAL_8250_DW is not set
#
# Non-8250 serial port support
#
# CONFIG_SERIAL_MAX3100 is not set
# CONFIG_SERIAL_MAX3107 is not set
CONFIG_SERIAL_CORE=y
CONFIG_SERIAL_CORE_CONSOLE=y
# CONFIG_SERIAL_OF_PLATFORM is not set
CONFIG_SERIAL_OMAP=y
CONFIG_SERIAL_OMAP_CONSOLE=y
# CONFIG_SERIAL_TIMBERDALE is not set
# CONFIG_SERIAL_ALTERA_JTAGUART is not set
# CONFIG_SERIAL_ALTERA_UART is not set
# CONFIG_SERIAL_IFX6X60 is not set
# CONFIG_SERIAL_XILINX_PS_UART is not set
# CONFIG_TTY_PRINTK is not set
# CONFIG_HVC_DCC is not set
# CONFIG_IPMI_HANDLER is not set
CONFIG_HW_RANDOM=y
# CONFIG_HW_RANDOM_TIMERIOMEM is not set
# CONFIG_NVRAM is not set
# CONFIG_R3964 is not set
# CONFIG_GPIO_DEVICE is not set
# CONFIG_RAW_DRIVER is not set
# CONFIG_TCG_TPM is not set
# CONFIG_RAMOOPS is not set
CONFIG_I2C=y
CONFIG_I2C_BOARDINFO=y
# CONFIG_I2C_COMPAT is not set
# CONFIG_I2C_CHARDEV is not set
# CONFIG_I2C_MUX is not set
# CONFIG_I2C_HELPER_AUTO is not set
# CONFIG_I2C_SMBUS is not set
#
# I2C Algorithms
#
# CONFIG_I2C_ALGOBIT is not set
# CONFIG_I2C_ALGOPCF is not set
# CONFIG_I2C_ALGOPCA is not set
#
# I2C Hardware Bus support
#
#
# I2C system bus drivers (mostly embedded / system-on-chip)
#
# CONFIG_I2C_DESIGNWARE_PLATFORM is not set
# CONFIG_I2C_GPIO is not set
# CONFIG_I2C_OCORES is not set
CONFIG_I2C_OMAP=y
# CONFIG_I2C_PCA_PLATFORM is not set
# CONFIG_I2C_PXA_PCI is not set
# CONFIG_I2C_SIMTEC is not set
# CONFIG_I2C_XILINX is not set
#
# External I2C/SMBus adapter drivers
#
# CONFIG_I2C_DIOLAN_U2C is not set
# CONFIG_I2C_PARPORT_LIGHT is not set
# CONFIG_I2C_TAOS_EVM is not set
# CONFIG_I2C_TINY_USB is not set
#
# Other I2C/SMBus bus drivers
#
# CONFIG_I2C_STUB is not set
# CONFIG_I2C_DEBUG_CORE is not set
# CONFIG_I2C_DEBUG_ALGO is not set
# CONFIG_I2C_DEBUG_BUS is not set
CONFIG_SPI=y
# CONFIG_SPI_DEBUG is not set
CONFIG_SPI_MASTER=y
#
# SPI Master Controller Drivers
#
# CONFIG_SPI_ALTERA is not set
# CONFIG_SPI_BITBANG is not set
# CONFIG_SPI_GPIO is not set
# CONFIG_SPI_GPIO_OLD is not set
# CONFIG_SPI_OC_TINY is not set
CONFIG_SPI_OMAP24XX=y
# CONFIG_SPI_PXA2XX_PCI is not set
# CONFIG_SPI_XILINX is not set
# CONFIG_SPI_DESIGNWARE is not set
#
# SPI Protocol Masters
#
# CONFIG_SPI_SPIDEV is not set
# CONFIG_SPI_TLE62X0 is not set
#
# PPS support
#
# CONFIG_PPS is not set
#
# PPS generators support
#
#
# PTP clock support
#
#
# Enable Device Drivers -> PPS to see the PTP clock options.
#
CONFIG_ARCH_REQUIRE_GPIOLIB=y
CONFIG_GPIOLIB=y
# CONFIG_DEBUG_GPIO is not set
CONFIG_GPIO_SYSFS=y
#
# Memory mapped GPIO drivers:
#
# CONFIG_GPIO_GENERIC_PLATFORM is not set
#
# I2C GPIO expanders:
#
# CONFIG_GPIO_MAX7300 is not set
# CONFIG_GPIO_MAX732X is not set
# CONFIG_GPIO_PCF857X is not set
# CONFIG_GPIO_SX150X is not set
# CONFIG_GPIO_TWL4030 is not set
# CONFIG_GPIO_ADP5588 is not set
#
# PCI GPIO expanders:
#
#
# SPI GPIO expanders:
#
# CONFIG_GPIO_MAX7301 is not set
# CONFIG_GPIO_MCP23S08 is not set
# CONFIG_GPIO_MC33880 is not set
# CONFIG_GPIO_74X164 is not set
#
# AC97 GPIO expanders:
#
#
# MODULbus GPIO expanders:
#
# CONFIG_W1 is not set
# CONFIG_POWER_SUPPLY is not set
# CONFIG_HWMON is not set
# CONFIG_THERMAL is not set
CONFIG_WATCHDOG=y
# CONFIG_WATCHDOG_CORE is not set
# CONFIG_WATCHDOG_NOWAYOUT is not set
#
# Watchdog Device Drivers
#
# CONFIG_SOFT_WATCHDOG is not set
# CONFIG_DW_WATCHDOG is not set
CONFIG_OMAP_WATCHDOG=y
# CONFIG_TWL4030_WATCHDOG is not set
# CONFIG_MAX63XX_WATCHDOG is not set
#
# USB-based Watchdog Cards
#
# CONFIG_USBPCWATCHDOG is not set
CONFIG_SSB_POSSIBLE=y
#
# Sonics Silicon Backplane
#
# CONFIG_SSB is not set
CONFIG_BCMA_POSSIBLE=y
#
# Broadcom specific AMBA
#
# CONFIG_BCMA is not set
#
# Multifunction device drivers
#
# CONFIG_MFD_CORE is not set
# CONFIG_MFD_88PM860X is not set
# CONFIG_MFD_SM501 is not set
# CONFIG_MFD_ASIC3 is not set
# CONFIG_HTC_EGPIO is not set
# CONFIG_HTC_PASIC3 is not set
# CONFIG_HTC_I2CPLD is not set
# CONFIG_TPS6105X is not set
# CONFIG_TPS65010 is not set
# CONFIG_TPS6507X is not set
# CONFIG_MFD_TPS6586X is not set
# CONFIG_MFD_TPS65910 is not set
# CONFIG_MFD_TPS65912_I2C is not set
# CONFIG_MFD_TPS65912_SPI is not set
CONFIG_TWL4030_CORE=y
# CONFIG_TWL4030_MADC is not set
CONFIG_TWL4030_POWER=y
# CONFIG_MFD_TWL4030_AUDIO is not set
# CONFIG_TWL6030_PWM is not set
# CONFIG_TWL6040_CORE is not set
# CONFIG_MFD_STMPE is not set
# CONFIG_MFD_TC3589X is not set
# CONFIG_MFD_TMIO is not set
# CONFIG_MFD_T7L66XB is not set
# CONFIG_MFD_TC6387XB is not set
# CONFIG_MFD_TC6393XB is not set
# CONFIG_PMIC_DA903X is not set
# CONFIG_MFD_DA9052_SPI is not set
# CONFIG_MFD_DA9052_I2C is not set
# CONFIG_PMIC_ADP5520 is not set
# CONFIG_MFD_MAX8925 is not set
# CONFIG_MFD_MAX8997 is not set
# CONFIG_MFD_MAX8998 is not set
# CONFIG_MFD_S5M_CORE is not set
# CONFIG_MFD_WM8400 is not set
# CONFIG_MFD_WM831X_I2C is not set
# CONFIG_MFD_WM831X_SPI is not set
# CONFIG_MFD_WM8350_I2C is not set
# CONFIG_MFD_WM8994 is not set
# CONFIG_MFD_PCF50633 is not set
# CONFIG_MFD_MC13XXX is not set
# CONFIG_ABX500_CORE is not set
# CONFIG_EZX_PCAP is not set
# CONFIG_MFD_WL1273_CORE is not set
CONFIG_MFD_OMAP_USB_HOST=y
# CONFIG_MFD_AAT2870_CORE is not set
CONFIG_REGULATOR=y
# CONFIG_REGULATOR_DEBUG is not set
CONFIG_REGULATOR_DUMMY=y
# CONFIG_REGULATOR_FIXED_VOLTAGE is not set
# CONFIG_REGULATOR_VIRTUAL_CONSUMER is not set
# CONFIG_REGULATOR_USERSPACE_CONSUMER is not set
# CONFIG_REGULATOR_GPIO is not set
# CONFIG_REGULATOR_BQ24022 is not set
# CONFIG_REGULATOR_MAX1586 is not set
# CONFIG_REGULATOR_MAX8649 is not set
# CONFIG_REGULATOR_MAX8660 is not set
# CONFIG_REGULATOR_MAX8952 is not set
# CONFIG_REGULATOR_TWL4030 is not set
# CONFIG_REGULATOR_LP3971 is not set
# CONFIG_REGULATOR_LP3972 is not set
# CONFIG_REGULATOR_TPS65023 is not set
# CONFIG_REGULATOR_TPS6507X is not set
# CONFIG_REGULATOR_ISL6271A is not set
# CONFIG_REGULATOR_AD5398 is not set
# CONFIG_REGULATOR_TPS6524X is not set
# CONFIG_MEDIA_SUPPORT is not set
#
# Graphics support
#
# CONFIG_DRM is not set
# CONFIG_VGASTATE is not set
# CONFIG_VIDEO_OUTPUT_CONTROL is not set
# CONFIG_FB is not set
# CONFIG_OMAP2_DSS is not set
# CONFIG_BACKLIGHT_LCD_SUPPORT is not set
# CONFIG_SOUND is not set
CONFIG_HID_SUPPORT=y
CONFIG_HID=y
CONFIG_HIDRAW=y
#
# USB Input Devices
#
# CONFIG_USB_HID is not set
# CONFIG_HID_PID is not set
#
# USB HID Boot Protocol drivers
#
# CONFIG_USB_KBD is not set
# CONFIG_USB_MOUSE is not set
#
# Special HID drivers
#
CONFIG_USB_SUPPORT=y
CONFIG_USB_COMMON=y
CONFIG_USB_ARCH_HAS_HCD=y
CONFIG_USB_ARCH_HAS_OHCI=y
CONFIG_USB_ARCH_HAS_EHCI=y
# CONFIG_USB_ARCH_HAS_XHCI is not set
CONFIG_USB=y
CONFIG_USB_DEBUG=y
CONFIG_USB_ANNOUNCE_NEW_DEVICES=y
#
# Miscellaneous USB options
#
# CONFIG_USB_DEVICEFS is not set
# CONFIG_USB_DEVICE_CLASS is not set
# CONFIG_USB_DYNAMIC_MINORS is not set
# CONFIG_USB_SUSPEND is not set
# CONFIG_USB_OTG_WHITELIST is not set
# CONFIG_USB_OTG_BLACKLIST_HUB is not set
# CONFIG_USB_DWC3 is not set
# CONFIG_USB_MON is not set
# CONFIG_USB_WUSB_CBAF is not set
#
# USB Host Controller Drivers
#
# CONFIG_USB_C67X00_HCD is not set
CONFIG_USB_EHCI_HCD=y
CONFIG_USB_EHCI_ROOT_HUB_TT=y
CONFIG_USB_EHCI_TT_NEWSCHED=y
CONFIG_USB_EHCI_HCD_OMAP=y
# CONFIG_USB_EHCI_MV is not set
# CONFIG_USB_OXU210HP_HCD is not set
# CONFIG_USB_ISP116X_HCD is not set
# CONFIG_USB_ISP1760_HCD is not set
# CONFIG_USB_ISP1362_HCD is not set
# CONFIG_USB_OHCI_HCD is not set
# CONFIG_USB_SL811_HCD is not set
# CONFIG_USB_R8A66597_HCD is not set
CONFIG_USB_MUSB_HDRC=y
# CONFIG_USB_MUSB_TUSB6010 is not set
CONFIG_USB_MUSB_OMAP2PLUS=y
# CONFIG_USB_MUSB_AM35X is not set
CONFIG_USB_INVENTRA_DMA=y
# CONFIG_MUSB_PIO_ONLY is not set
# CONFIG_USB_RENESAS_USBHS is not set
#
# USB Device Class drivers
#
# CONFIG_USB_ACM is not set
# CONFIG_USB_PRINTER is not set
# CONFIG_USB_WDM is not set
# CONFIG_USB_TMC is not set
#
# NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may
#
#
# also be needed; see USB_STORAGE Help for more info
#
CONFIG_USB_STORAGE=m
# CONFIG_USB_STORAGE_DEBUG is not set
# CONFIG_USB_STORAGE_REALTEK is not set
# CONFIG_USB_STORAGE_DATAFAB is not set
# CONFIG_USB_STORAGE_FREECOM is not set
# CONFIG_USB_STORAGE_ISD200 is not set
# CONFIG_USB_STORAGE_USBAT is not set
# CONFIG_USB_STORAGE_SDDR09 is not set
# CONFIG_USB_STORAGE_SDDR55 is not set
# CONFIG_USB_STORAGE_JUMPSHOT is not set
# CONFIG_USB_STORAGE_ALAUDA is not set
# CONFIG_USB_STORAGE_ONETOUCH is not set
# CONFIG_USB_STORAGE_KARMA is not set
# CONFIG_USB_STORAGE_CYPRESS_ATACB is not set
# CONFIG_USB_STORAGE_ENE_UB6250 is not set
# CONFIG_USB_UAS is not set
# CONFIG_USB_LIBUSUAL is not set
#
# USB Imaging devices
#
# CONFIG_USB_MDC800 is not set
# CONFIG_USB_MICROTEK is not set
#
# USB port drivers
#
# CONFIG_USB_SERIAL is not set
#
# USB Miscellaneous drivers
#
# CONFIG_USB_EMI62 is not set
# CONFIG_USB_EMI26 is not set
# CONFIG_USB_ADUTUX is not set
# CONFIG_USB_SEVSEG is not set
# CONFIG_USB_RIO500 is not set
# CONFIG_USB_LEGOTOWER is not set
# CONFIG_USB_LCD is not set
# CONFIG_USB_LED is not set
# CONFIG_USB_CYPRESS_CY7C63 is not set
# CONFIG_USB_CYTHERM is not set
# CONFIG_USB_IDMOUSE is not set
# CONFIG_USB_FTDI_ELAN is not set
# CONFIG_USB_APPLEDISPLAY is not set
# CONFIG_USB_SISUSBVGA is not set
# CONFIG_USB_LD is not set
# CONFIG_USB_TRANCEVIBRATOR is not set
# CONFIG_USB_IOWARRIOR is not set
CONFIG_USB_TEST=y
# CONFIG_USB_ISIGHTFW is not set
# CONFIG_USB_YUREX is not set
CONFIG_USB_GADGET=y
CONFIG_USB_GADGET_DEBUG=y
# CONFIG_USB_GADGET_DEBUG_FILES is not set
# CONFIG_USB_GADGET_DEBUG_FS is not set
CONFIG_USB_GADGET_VBUS_DRAW=500
CONFIG_USB_GADGET_STORAGE_NUM_BUFFERS=2
# CONFIG_USB_FUSB300 is not set
# CONFIG_USB_OMAP is not set
# CONFIG_USB_R8A66597 is not set
# CONFIG_USB_MV_UDC is not set
CONFIG_USB_GADGET_MUSB_HDRC=y
# CONFIG_USB_M66592 is not set
# CONFIG_USB_NET2272 is not set
# CONFIG_USB_DUMMY_HCD is not set
CONFIG_USB_GADGET_DUALSPEED=y
# CONFIG_USB_ZERO is not set
# CONFIG_USB_ETH is not set
# CONFIG_USB_G_NCM is not set
CONFIG_USB_GADGETFS=m
# CONFIG_USB_FUNCTIONFS is not set
# CONFIG_USB_FILE_STORAGE is not set
# CONFIG_USB_MASS_STORAGE is not set
CONFIG_USB_G_SERIAL=m
# CONFIG_USB_G_PRINTER is not set
# CONFIG_USB_CDC_COMPOSITE is not set
# CONFIG_USB_G_ACM_MS is not set
# CONFIG_USB_G_MULTI is not set
# CONFIG_USB_G_HID is not set
# CONFIG_USB_G_DBGP is not set
#
# OTG and related infrastructure
#
CONFIG_USB_OTG_UTILS=y
# CONFIG_USB_GPIO_VBUS is not set
# CONFIG_ISP1301_OMAP is not set
CONFIG_USB_ULPI=y
# CONFIG_TWL6030_USB is not set
CONFIG_NOP_USB_XCEIV=y
CONFIG_MMC=y
# CONFIG_MMC_DEBUG is not set
# CONFIG_MMC_UNSAFE_RESUME is not set
# CONFIG_MMC_CLKGATE is not set
#
# MMC/SD/SDIO Card Drivers
#
# CONFIG_MMC_BLOCK is not set
CONFIG_SDIO_UART=y
# CONFIG_MMC_TEST is not set
#
# MMC/SD/SDIO Host Controller Drivers
#
# CONFIG_MMC_SDHCI is not set
# CONFIG_MMC_SDHCI_PXAV3 is not set
# CONFIG_MMC_SDHCI_PXAV2 is not set
# CONFIG_MMC_OMAP is not set
# CONFIG_MMC_OMAP_HS is not set
# CONFIG_MMC_DW is not set
# CONFIG_MMC_VUB300 is not set
# CONFIG_MMC_USHC is not set
# CONFIG_MEMSTICK is not set
CONFIG_NEW_LEDS=y
CONFIG_LEDS_CLASS=y
#
# LED drivers
#
# CONFIG_LEDS_LM3530 is not set
# CONFIG_LEDS_PCA9532 is not set
# CONFIG_LEDS_GPIO is not set
# CONFIG_LEDS_LP3944 is not set
# CONFIG_LEDS_LP5521 is not set
# CONFIG_LEDS_LP5523 is not set
# CONFIG_LEDS_PCA955X is not set
# CONFIG_LEDS_DAC124S085 is not set
# CONFIG_LEDS_REGULATOR is not set
# CONFIG_LEDS_BD2802 is not set
# CONFIG_LEDS_LT3593 is not set
# CONFIG_LEDS_RENESAS_TPU is not set
# CONFIG_LEDS_TCA6507 is not set
# CONFIG_LEDS_OT200 is not set
CONFIG_LEDS_TRIGGERS=y
#
# LED Triggers
#
CONFIG_LEDS_TRIGGER_TIMER=y
# CONFIG_LEDS_TRIGGER_HEARTBEAT is not set
# CONFIG_LEDS_TRIGGER_BACKLIGHT is not set
# CONFIG_LEDS_TRIGGER_GPIO is not set
CONFIG_LEDS_TRIGGER_DEFAULT_ON=y
#
# iptables trigger is under Netfilter config (LED target)
#
# CONFIG_LEDS_TRIGGER_MORSE is not set
CONFIG_LEDS_TRIGGER_NETDEV=y
# CONFIG_LEDS_TRIGGER_USBDEV is not set
# CONFIG_ACCESSIBILITY is not set
CONFIG_RTC_LIB=y
CONFIG_RTC_CLASS=y
CONFIG_RTC_HCTOSYS=y
CONFIG_RTC_HCTOSYS_DEVICE="rtc0"
# CONFIG_RTC_DEBUG is not set
#
# RTC interfaces
#
CONFIG_RTC_INTF_SYSFS=y
CONFIG_RTC_INTF_PROC=y
CONFIG_RTC_INTF_DEV=y
# CONFIG_RTC_INTF_DEV_UIE_EMUL is not set
# CONFIG_RTC_DRV_TEST is not set
#
# I2C RTC drivers
#
# CONFIG_RTC_DRV_DS1307 is not set
# CONFIG_RTC_DRV_DS1374 is not set
# CONFIG_RTC_DRV_DS1672 is not set
# CONFIG_RTC_DRV_DS3232 is not set
# CONFIG_RTC_DRV_MAX6900 is not set
# CONFIG_RTC_DRV_RS5C372 is not set
# CONFIG_RTC_DRV_ISL1208 is not set
# CONFIG_RTC_DRV_ISL12022 is not set
# CONFIG_RTC_DRV_X1205 is not set
# CONFIG_RTC_DRV_PCF8563 is not set
# CONFIG_RTC_DRV_PCF8583 is not set
# CONFIG_RTC_DRV_M41T80 is not set
# CONFIG_RTC_DRV_BQ32K is not set
# CONFIG_RTC_DRV_TWL4030 is not set
# CONFIG_RTC_DRV_S35390A is not set
# CONFIG_RTC_DRV_FM3130 is not set
# CONFIG_RTC_DRV_RX8581 is not set
# CONFIG_RTC_DRV_RX8025 is not set
# CONFIG_RTC_DRV_EM3027 is not set
# CONFIG_RTC_DRV_RV3029C2 is not set
# CONFIG_RTC_DRV_PT7C4338 is not set
#
# SPI RTC drivers
#
# CONFIG_RTC_DRV_M41T93 is not set
# CONFIG_RTC_DRV_M41T94 is not set
# CONFIG_RTC_DRV_DS1305 is not set
# CONFIG_RTC_DRV_DS1390 is not set
# CONFIG_RTC_DRV_MAX6902 is not set
# CONFIG_RTC_DRV_R9701 is not set
# CONFIG_RTC_DRV_RS5C348 is not set
# CONFIG_RTC_DRV_DS3234 is not set
# CONFIG_RTC_DRV_PCF2123 is not set
#
# Platform RTC drivers
#
CONFIG_RTC_DRV_CMOS=y
# CONFIG_RTC_DRV_DS1286 is not set
# CONFIG_RTC_DRV_DS1511 is not set
# CONFIG_RTC_DRV_DS1553 is not set
# CONFIG_RTC_DRV_DS1742 is not set
# CONFIG_RTC_DRV_STK17TA8 is not set
# CONFIG_RTC_DRV_M48T86 is not set
# CONFIG_RTC_DRV_M48T35 is not set
# CONFIG_RTC_DRV_M48T59 is not set
# CONFIG_RTC_DRV_MSM6242 is not set
# CONFIG_RTC_DRV_BQ4802 is not set
# CONFIG_RTC_DRV_RP5C01 is not set
# CONFIG_RTC_DRV_V3020 is not set
# CONFIG_RTC_DRV_RTC7301 is not set
#
# on-CPU RTC drivers
#
# CONFIG_DMADEVICES is not set
# CONFIG_AUXDISPLAY is not set
CONFIG_UIO=y
# CONFIG_UIO_PDRV is not set
# CONFIG_UIO_PDRV_GENIRQ is not set
#
# Virtio drivers
#
# CONFIG_VIRTIO_BALLOON is not set
# CONFIG_VIRTIO_MMIO is not set
#
# Microsoft Hyper-V guest support
#
# CONFIG_STAGING is not set
CONFIG_CLKDEV_LOOKUP=y
#
# Hardware Spinlock drivers
#
CONFIG_CLKSRC_MMIO=y
# CONFIG_IOMMU_SUPPORT is not set
# CONFIG_VIRT_DRIVERS is not set
# CONFIG_PM_DEVFREQ is not set
#
# File systems
#
# CONFIG_EXT2_FS is not set
CONFIG_EXT3_FS=y
# CONFIG_EXT3_DEFAULTS_TO_ORDERED is not set
CONFIG_EXT3_FS_XATTR=y
# CONFIG_EXT3_FS_POSIX_ACL is not set
# CONFIG_EXT3_FS_SECURITY is not set
CONFIG_EXT4_FS=y
CONFIG_EXT4_USE_FOR_EXT23=y
CONFIG_EXT4_FS_XATTR=y
CONFIG_EXT4_FS_POSIX_ACL=y
CONFIG_EXT4_FS_SECURITY=y
CONFIG_EXT4_DEBUG=y
CONFIG_JBD=y
# CONFIG_JBD_DEBUG is not set
CONFIG_JBD2=y
# CONFIG_JBD2_DEBUG is not set
CONFIG_FS_MBCACHE=y
# CONFIG_REISERFS_FS is not set
# CONFIG_JFS_FS is not set
# CONFIG_XFS_FS is not set
# CONFIG_GFS2_FS is not set
# CONFIG_BTRFS_FS is not set
# CONFIG_NILFS2_FS is not set
CONFIG_FS_POSIX_ACL=y
CONFIG_FILE_LOCKING=y
CONFIG_FSNOTIFY=y
# CONFIG_DNOTIFY is not set
CONFIG_INOTIFY_USER=y
# CONFIG_FANOTIFY is not set
# CONFIG_QUOTA is not set
# CONFIG_QUOTACTL is not set
CONFIG_AUTOFS4_FS=m
# CONFIG_FUSE_FS is not set
CONFIG_OVERLAYFS_FS=y
#
# Caches
#
# CONFIG_FSCACHE is not set
#
# CD-ROM/DVD Filesystems
#
# CONFIG_ISO9660_FS is not set
# CONFIG_UDF_FS is not set
#
# DOS/FAT/NT Filesystems
#
# CONFIG_MSDOS_FS is not set
# CONFIG_VFAT_FS is not set
# CONFIG_NTFS_FS is not set
#
# Pseudo filesystems
#
CONFIG_PROC_FS=y
CONFIG_PROC_SYSCTL=y
# CONFIG_PROC_PAGE_MONITOR is not set
CONFIG_SYSFS=y
CONFIG_TMPFS=y
# CONFIG_TMPFS_POSIX_ACL is not set
CONFIG_TMPFS_XATTR=y
# CONFIG_HUGETLB_PAGE is not set
# CONFIG_CONFIGFS_FS is not set
CONFIG_MISC_FILESYSTEMS=y
# CONFIG_ADFS_FS is not set
# CONFIG_AFFS_FS is not set
# CONFIG_HFS_FS is not set
# CONFIG_HFSPLUS_FS is not set
# CONFIG_BEFS_FS is not set
# CONFIG_BFS_FS is not set
# CONFIG_EFS_FS is not set
# CONFIG_YAFFS_FS is not set
CONFIG_JFFS2_FS=y
CONFIG_JFFS2_FS_DEBUG=0
CONFIG_JFFS2_FS_WRITEBUFFER=y
# CONFIG_JFFS2_FS_WBUF_VERIFY is not set
CONFIG_JFFS2_SUMMARY=y
CONFIG_JFFS2_FS_XATTR=y
# CONFIG_JFFS2_FS_POSIX_ACL is not set
# CONFIG_JFFS2_FS_SECURITY is not set
CONFIG_JFFS2_COMPRESSION_OPTIONS=y
# CONFIG_JFFS2_ZLIB is not set
# CONFIG_JFFS2_LZO is not set
CONFIG_JFFS2_LZMA=y
CONFIG_JFFS2_RTIME=y
# CONFIG_JFFS2_RUBIN is not set
# CONFIG_JFFS2_CMODE_NONE is not set
CONFIG_JFFS2_CMODE_PRIORITY=y
# CONFIG_JFFS2_CMODE_SIZE is not set
# CONFIG_JFFS2_CMODE_FAVOURLZO is not set
# CONFIG_LOGFS is not set
# CONFIG_CRAMFS is not set
CONFIG_SQUASHFS=y
# CONFIG_SQUASHFS_XATTR is not set
# CONFIG_SQUASHFS_ZLIB is not set
# CONFIG_SQUASHFS_LZO is not set
CONFIG_SQUASHFS_XZ=y
# CONFIG_SQUASHFS_4K_DEVBLK_SIZE is not set
# CONFIG_SQUASHFS_EMBEDDED is not set
CONFIG_SQUASHFS_FRAGMENT_CACHE_SIZE=3
# CONFIG_VXFS_FS is not set
# CONFIG_MINIX_FS is not set
# CONFIG_OMFS_FS is not set
# CONFIG_HPFS_FS is not set
# CONFIG_QNX4FS_FS is not set
# CONFIG_ROMFS_FS is not set
# CONFIG_PSTORE is not set
# CONFIG_SYSV_FS is not set
# CONFIG_UFS_FS is not set
CONFIG_NETWORK_FILESYSTEMS=y
# CONFIG_NFS_FS is not set
# CONFIG_NFSD is not set
# CONFIG_CEPH_FS is not set
# CONFIG_CIFS is not set
# CONFIG_NCP_FS is not set
# CONFIG_CODA_FS is not set
# CONFIG_AFS_FS is not set
CONFIG_NLS=y
CONFIG_NLS_DEFAULT="iso8859-1"
# CONFIG_NLS_CODEPAGE_437 is not set
# CONFIG_NLS_CODEPAGE_737 is not set
# CONFIG_NLS_CODEPAGE_775 is not set
# CONFIG_NLS_CODEPAGE_850 is not set
# CONFIG_NLS_CODEPAGE_852 is not set
# CONFIG_NLS_CODEPAGE_855 is not set
# CONFIG_NLS_CODEPAGE_857 is not set
# CONFIG_NLS_CODEPAGE_860 is not set
# CONFIG_NLS_CODEPAGE_861 is not set
# CONFIG_NLS_CODEPAGE_862 is not set
# CONFIG_NLS_CODEPAGE_863 is not set
# CONFIG_NLS_CODEPAGE_864 is not set
# CONFIG_NLS_CODEPAGE_865 is not set
# CONFIG_NLS_CODEPAGE_866 is not set
# CONFIG_NLS_CODEPAGE_869 is not set
# CONFIG_NLS_CODEPAGE_936 is not set
# CONFIG_NLS_CODEPAGE_950 is not set
# CONFIG_NLS_CODEPAGE_932 is not set
# CONFIG_NLS_CODEPAGE_949 is not set
# CONFIG_NLS_CODEPAGE_874 is not set
# CONFIG_NLS_ISO8859_8 is not set
# CONFIG_NLS_CODEPAGE_1250 is not set
# CONFIG_NLS_CODEPAGE_1251 is not set
# CONFIG_NLS_ASCII is not set
# CONFIG_NLS_ISO8859_1 is not set
# CONFIG_NLS_ISO8859_2 is not set
# CONFIG_NLS_ISO8859_3 is not set
# CONFIG_NLS_ISO8859_4 is not set
# CONFIG_NLS_ISO8859_5 is not set
# CONFIG_NLS_ISO8859_6 is not set
# CONFIG_NLS_ISO8859_7 is not set
# CONFIG_NLS_ISO8859_9 is not set
# CONFIG_NLS_ISO8859_13 is not set
# CONFIG_NLS_ISO8859_14 is not set
# CONFIG_NLS_ISO8859_15 is not set
# CONFIG_NLS_KOI8_R is not set
# CONFIG_NLS_KOI8_U is not set
# CONFIG_NLS_UTF8 is not set
#
# Kernel hacking
#
CONFIG_PRINTK_TIME=y
CONFIG_DEFAULT_MESSAGE_LOGLEVEL=4
CONFIG_ENABLE_WARN_DEPRECATED=y
# CONFIG_ENABLE_MUST_CHECK is not set
CONFIG_FRAME_WARN=1024
CONFIG_MAGIC_SYSRQ=y
CONFIG_STRIP_ASM_SYMS=y
# CONFIG_UNUSED_SYMBOLS is not set
CONFIG_DEBUG_FS=y
# CONFIG_HEADERS_CHECK is not set
# CONFIG_DEBUG_SECTION_MISMATCH is not set
CONFIG_DEBUG_KERNEL=y
# CONFIG_DEBUG_SHIRQ is not set
# CONFIG_LOCKUP_DETECTOR is not set
# CONFIG_HARDLOCKUP_DETECTOR is not set
# CONFIG_DETECT_HUNG_TASK is not set
# CONFIG_SCHED_DEBUG is not set
# CONFIG_SCHEDSTATS is not set
# CONFIG_TIMER_STATS is not set
# CONFIG_DEBUG_OBJECTS is not set
# CONFIG_DEBUG_SLAB is not set
# CONFIG_DEBUG_KMEMLEAK is not set
# CONFIG_DEBUG_PREEMPT is not set
# CONFIG_DEBUG_RT_MUTEXES is not set
# CONFIG_RT_MUTEX_TESTER is not set
# CONFIG_DEBUG_SPINLOCK is not set
# CONFIG_DEBUG_MUTEXES is not set
# CONFIG_DEBUG_LOCK_ALLOC is not set
# CONFIG_PROVE_LOCKING is not set
# CONFIG_SPARSE_RCU_POINTER is not set
# CONFIG_LOCK_STAT is not set
# CONFIG_DEBUG_ATOMIC_SLEEP is not set
# CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set
# CONFIG_DEBUG_STACK_USAGE is not set
# CONFIG_DEBUG_KOBJECT is not set
# CONFIG_DEBUG_HIGHMEM is not set
# CONFIG_DEBUG_BUGVERBOSE is not set
CONFIG_DEBUG_INFO=y
CONFIG_DEBUG_INFO_REDUCED=y
# CONFIG_DEBUG_VM is not set
# CONFIG_DEBUG_WRITECOUNT is not set
# CONFIG_DEBUG_MEMORY_INIT is not set
# CONFIG_DEBUG_LIST is not set
# CONFIG_TEST_LIST_SORT is not set
# CONFIG_DEBUG_SG is not set
# CONFIG_DEBUG_NOTIFIERS is not set
# CONFIG_DEBUG_CREDENTIALS is not set
CONFIG_FRAME_POINTER=y
# CONFIG_BOOT_PRINTK_DELAY is not set
# CONFIG_RCU_TORTURE_TEST is not set
# CONFIG_BACKTRACE_SELF_TEST is not set
# CONFIG_DEBUG_BLOCK_EXT_DEVT is not set
# CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set
# CONFIG_LKDTM is not set
# CONFIG_FAULT_INJECTION is not set
# CONFIG_LATENCYTOP is not set
# CONFIG_SYSCTL_SYSCALL_CHECK is not set
# CONFIG_DEBUG_PAGEALLOC is not set
CONFIG_HAVE_FUNCTION_TRACER=y
CONFIG_HAVE_FUNCTION_GRAPH_TRACER=y
CONFIG_HAVE_DYNAMIC_FTRACE=y
CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y
CONFIG_HAVE_C_RECORDMCOUNT=y
CONFIG_TRACING_SUPPORT=y
# CONFIG_FTRACE is not set
CONFIG_DYNAMIC_DEBUG=y
# CONFIG_DMA_API_DEBUG is not set
# CONFIG_ATOMIC64_SELFTEST is not set
# CONFIG_SAMPLES is not set
CONFIG_HAVE_ARCH_KGDB=y
# CONFIG_KGDB is not set
# CONFIG_TEST_KSTRTOX is not set
# CONFIG_STRICT_DEVMEM is not set
# CONFIG_ARM_UNWIND is not set
# CONFIG_DEBUG_USER is not set
CONFIG_DEBUG_LL=y
CONFIG_DEBUG_LL_UART_NONE=y
# CONFIG_DEBUG_ICEDCC is not set
CONFIG_EARLY_PRINTK=y
#
# Security options
#
# CONFIG_KEYS is not set
# CONFIG_SECURITY_DMESG_RESTRICT is not set
# CONFIG_SECURITY is not set
# CONFIG_SECURITYFS is not set
CONFIG_DEFAULT_SECURITY_DAC=y
CONFIG_DEFAULT_SECURITY=""
CONFIG_CRYPTO=y
#
# Crypto core or helper
#
CONFIG_CRYPTO_ALGAPI=y
CONFIG_CRYPTO_ALGAPI2=y
# CONFIG_CRYPTO_AEAD is not set
CONFIG_CRYPTO_AEAD2=y
CONFIG_CRYPTO_BLKCIPHER=y
CONFIG_CRYPTO_BLKCIPHER2=y
CONFIG_CRYPTO_HASH=y
CONFIG_CRYPTO_HASH2=y
# CONFIG_CRYPTO_RNG is not set
CONFIG_CRYPTO_RNG2=y
CONFIG_CRYPTO_PCOMP=y
CONFIG_CRYPTO_PCOMP2=y
CONFIG_CRYPTO_MANAGER=y
CONFIG_CRYPTO_MANAGER2=y
# CONFIG_CRYPTO_USER is not set
CONFIG_CRYPTO_MANAGER_DISABLE_TESTS=y
# CONFIG_CRYPTO_GF128MUL is not set
# CONFIG_CRYPTO_NULL is not set
CONFIG_CRYPTO_WORKQUEUE=y
# CONFIG_CRYPTO_CRYPTD is not set
# CONFIG_CRYPTO_AUTHENC is not set
# CONFIG_CRYPTO_TEST is not set
#
# Authenticated Encryption with Associated Data
#
# CONFIG_CRYPTO_CCM is not set
# CONFIG_CRYPTO_GCM is not set
# CONFIG_CRYPTO_SEQIV is not set
#
# Block modes
#
CONFIG_CRYPTO_CBC=y
# CONFIG_CRYPTO_CTR is not set
# CONFIG_CRYPTO_CTS is not set
# CONFIG_CRYPTO_ECB is not set
# CONFIG_CRYPTO_LRW is not set
# CONFIG_CRYPTO_PCBC is not set
# CONFIG_CRYPTO_XTS is not set
#
# Hash modes
#
# CONFIG_CRYPTO_HMAC is not set
# CONFIG_CRYPTO_XCBC is not set
# CONFIG_CRYPTO_VMAC is not set
#
# Digest
#
CONFIG_CRYPTO_CRC32C=y
# CONFIG_CRYPTO_GHASH is not set
# CONFIG_CRYPTO_MD4 is not set
CONFIG_CRYPTO_MD5=y
CONFIG_CRYPTO_MICHAEL_MIC=y
# CONFIG_CRYPTO_RMD128 is not set
# CONFIG_CRYPTO_RMD160 is not set
# CONFIG_CRYPTO_RMD256 is not set
# CONFIG_CRYPTO_RMD320 is not set
# CONFIG_CRYPTO_SHA1 is not set
# CONFIG_CRYPTO_SHA256 is not set
# CONFIG_CRYPTO_SHA512 is not set
# CONFIG_CRYPTO_TGR192 is not set
# CONFIG_CRYPTO_WP512 is not set
#
# Ciphers
#
CONFIG_CRYPTO_AES=y
# CONFIG_CRYPTO_ANUBIS is not set
CONFIG_CRYPTO_ARC4=m
# CONFIG_CRYPTO_BLOWFISH is not set
# CONFIG_CRYPTO_CAMELLIA is not set
# CONFIG_CRYPTO_CAST5 is not set
# CONFIG_CRYPTO_CAST6 is not set
CONFIG_CRYPTO_DES=y
# CONFIG_CRYPTO_FCRYPT is not set
# CONFIG_CRYPTO_KHAZAD is not set
# CONFIG_CRYPTO_SALSA20 is not set
# CONFIG_CRYPTO_SEED is not set
# CONFIG_CRYPTO_SERPENT is not set
# CONFIG_CRYPTO_TEA is not set
# CONFIG_CRYPTO_TWOFISH is not set
#
# Compression
#
# CONFIG_CRYPTO_DEFLATE is not set
CONFIG_CRYPTO_ZLIB=y
# CONFIG_CRYPTO_LZO is not set
# CONFIG_CRYPTO_XZ is not set
#
# Random Number Generation
#
# CONFIG_CRYPTO_ANSI_CPRNG is not set
# CONFIG_CRYPTO_USER_API_HASH is not set
# CONFIG_CRYPTO_USER_API_SKCIPHER is not set
CONFIG_CRYPTO_HW=y
# CONFIG_CRYPTO_DEV_OMAP_SHAM is not set
# CONFIG_CRYPTO_DEV_OMAP_AES is not set
#
# OCF Configuration
#
# CONFIG_OCF_OCF is not set
# CONFIG_BINARY_PRINTF is not set
#
# Library routines
#
CONFIG_BITREVERSE=y
CONFIG_GENERIC_PCI_IOMAP=y
CONFIG_CRC_CCITT=y
CONFIG_CRC16=y
# CONFIG_CRC_T10DIF is not set
CONFIG_CRC_ITU_T=m
CONFIG_CRC32=y
# CONFIG_CRC7 is not set
CONFIG_LIBCRC32C=y
# CONFIG_CRC8 is not set
CONFIG_ZLIB_INFLATE=y
CONFIG_ZLIB_DEFLATE=y
CONFIG_XZ_DEC=y
# CONFIG_XZ_DEC_X86 is not set
# CONFIG_XZ_DEC_POWERPC is not set
# CONFIG_XZ_DEC_IA64 is not set
# CONFIG_XZ_DEC_ARM is not set
# CONFIG_XZ_DEC_ARMTHUMB is not set
# CONFIG_XZ_DEC_SPARC is not set
# CONFIG_XZ_DEC_BCJ is not set
# CONFIG_XZ_DEC_TEST is not set
CONFIG_LZMA_COMPRESS=y
CONFIG_LZMA_DECOMPRESS=y
CONFIG_DECOMPRESS_LZMA=y
CONFIG_TEXTSEARCH=y
# CONFIG_TEXTSEARCH_KMP is not set
# CONFIG_TEXTSEARCH_BM is not set
# CONFIG_TEXTSEARCH_FSM is not set
CONFIG_HAS_IOMEM=y
CONFIG_HAS_IOPORT=y
CONFIG_HAS_DMA=y
CONFIG_DQL=y
CONFIG_NLATTR=y
CONFIG_AVERAGE=y
# CONFIG_CORDIC is not set