This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

my dsp application gets stuck saying entering RPC_recvMesg()



Hi,

I have downloaded c6run_0_98_03_03. I built the example applications given in c6runlib. I generated cfft_dsp file. while running the application in debug mode it says RPC_IPC_recvMsg() and gets stuck at that point. I used the following as my bootargs

setenv optargs mem=80M@0x80000000 mem=384M@0x88000000

I loaded the cmemk.ko module using the following command

insmod cmemk.ko phys_start=0x858e7000 pools=1x4096  phys_end=0x87900000 allowOverlap=1

I am attaching the code with this mail. I would also like to know how I can increase the memory available to DSP. I could not reduce the value of phys_start

5483.emqbit.zip

Thanks!!!