Hi all,
Based on android 4.0, can I set the max bits per frame for H264?
In low bit rate network environment, some H264 frames are even larger than 100k bits when the encoder is in default settings.
And at this case, it can encode only 1-2 frames per second.
So I want to set the max size of the the frame.But I can't find relevant parameters.
Thx
regards,
changwenliang