This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

gst-openmax and openmax on ics and omap 4



Hi, everyone!

       I want to use the gst-openmax and omx_h264enc  to encode the yuv file on the ics and omap4.   the omx_h264enc  can encode the file  but the result  file  can not play by the player on pc. and  i  find  there is no sps and pps in this  file . alsa  i find   the  omap4  colorformat  is OMX_TI_COLOR_FormatYUV420PackedSemiPlanar.  i want  to set the colorformat of the encoder  to OMX_COLOR_FormatYUV420PackedSemiPlanar  ,but  i  failed     i  read  colorformat   of  the  in port  also  OMX_TI_COLOR_FormatYUV420PackedSemiPlanar . Can  this  omap4  only  support  the OMX_TI_COLOR_FormatYUV420PackedSemiPlanar  colorformat ?If  that is true ,  i  want to   give  the OMX_TI_COLOR_FormatYUV420PackedSemiPlanar  to encoder . What  format of yuv about the OMX_TI_COLOR_FormatYUV420PackedSemiPlanar ?

the  code  is below:

                G_OMX_PORT_GET_DEFINITION (omx_base->in_port, &param);
                dumpPortStatus(omx_base->in_port);/*****ADD******/
                width = param.format.video.nFrameWidth;
                height = param.format.video.nFrameHeight;
                framerate = param.format.video.xFramerate;
                param.format.video.nStride = 1280;
                param.format.video.eColorFormat = OMX_COLOR_FormatYUV420PackedSemiPlanar;
                /* this is against the standard; nBufferSize is read-only. */
                fourcc = g_omx_colorformat_to_fourcc (param.format.video.eColorFormat);
                param.nBufferSize = gst_video_format_get_size_strided (
                        gst_video_format_from_fourcc (fourcc),
                        width, height, param.format.video.nStride);
                error_val = G_OMX_PORT_SET_DEFINITION (omx_base->in_port, &param);
                dumpPortStatus(omx_base->in_port);

Thank you very much!

  • In a test way you can use code for example from Android source code in 4AI1.4.P1,

    http://git.omapzoom.org/?p=platform/frameworks/base.git;a=blob;f=media/libstagefright/OMXCodec.cpp;h=60d9bb727800c4a6c56fbdbe6ef889fc9700aae7;hb=refs/heads/master

    ./mydroid/frameworks/base/media/libstagefright/OMXCodec.cpp

    status_t OMXCodec::isColorFormatSupported(
            OMX_COLOR_FORMATTYPE colorFormat, int portIndex) {

    and check that you are setting correct index in your code, and some variables seems to be copied at the other side, try to put them in left side

    you could try to use next function's code as reference, it is in the same file

    void OMXCodec::setVideoInputFormat(
            const char *mime, const sp<MetaData>& meta) {

    and in case it doesn't fix the issue, could you add some logs about actual error to check what error is being returned? and you are using Android, what release are you using? can you provide code at the surroundings of shared code? like code where port index is added before calling OMX_GetParameter.

    check http://e2e.ti.com/support/omap/f/849/t/179160.aspx for more information about what posts must contain.

    You can use get some debug prints using information from next link

    http://omapedia.org/wiki/Debugging_RPMsg

  • Hi,  Manuel:

         Thank you for your  answer.  The version of ics   is  4.0.3。  The  gstreamer  command  is "gst-launch -v filesrc location=/mnt/ext_sdcard/nv12.yuv ! videoparse width=1280 height=720 ! omx_h264enc ! filesink location=/mnt/sdcard/test1.264 --gst-debug=omx:5".  I use  the  ./mydroid/frameworks/base/media/libstagefright/OMXCodec.cppstatus_t OMXCodec::isColorFormatSupported(OMX_COLOR_FORMATTYPE colorFormat, int portIndex)    it  can  support  the color format  of  OMX_TI_COLOR_FormatYUV420PackedSemiPlanar .  but  it  is not support  OMX_COLOR_FormatYUV420PackedSemiPlanar.so  i can not  understand  .I  use the movie  editor  apk  and  it can  encode mp4 file  successful. the movie editor  also  use  openmax  .and  in  the source code  hardware/ti/domx/omx_proxy_component/omx_h264_enc/src/omx_proxy_common.c  

    OMX_ERRORTYPE LOCAL_PROXY_H264E_SetParameter(OMX_IN OMX_HANDLETYPE hComponent, OMX_IN OMX_INDEXTYPE nParamIndex, OMX_IN OMX_PTR pParamStruct)

    if(nParamIndex == OMX_IndexParamPortDefinition)
        {
            pPortDef = (OMX_PARAM_PORTDEFINITIONTYPE *)pParamStruct;
            if(pPortDef->format.video.eColorFormat == OMX_TI_COLOR_FormatYUV420PackedSemiPlanar)
            {
                pPortDef->format.video.eColorFormat = OMX_COLOR_FormatYUV420PackedSemiPlanar;
            }
    #ifdef ANDROID_CUSTOM_OPAQUECOLORFORMAT
            else if(pPortDef->format.video.eColorFormat == OMX_COLOR_FormatAndroidOpaque)
            {
                if(COLORCONVERT_open(&pProxy->hCC,pCompPrv) != 0)
                {
                    PROXY_assert(0, OMX_ErrorInsufficientResources,
                                "Failed to open Color converting service");
                }
                pProxy->bAndroidOpaqueFormat = OMX_TRUE;
                pPortDef->format.video.eColorFormat = OMX_COLOR_FormatYUV420PackedSemiPlanar;
            }
    #endif

    I  think  it will  covert  OMX_TI_COLOR_FormatYUV420PackedSemiPlanar  to  OMX_COLOR_FormatYUV420PackedSemiPlanar. Is  it  effect? and  i  set  the  parameter


                    param.format.video.eColorFormat = OMX_COLOR_FormatYUV420PackedSemiPlanar;
                  
                    /* this is against the standard; nBufferSize is read-only. */
                    fourcc = g_omx_colorformat_to_fourcc (param.format.video.eColorFormat);
                    param.nBufferSize = gst_video_format_get_size_strided (
                            gst_video_format_from_fourcc (fourcc),
                            width, height, param.format.video.nStride);
                    error_val = G_OMX_PORT_SET_DEFINITION (omx_base->in_port, &param);
                    GST_DEBUG_OBJECT(omx_base," error_val = %x\n",,error_val);/*****ADD******/
                    dumpPortStatus(omx_base->in_port);
             
        the  log is 

    Input Port  

    eCompressionFormat = OMX_VIDEO_CodingUnused

    eColorFormat = OMX_TI_COLOR_FormatYUV420PackedSemiPlanar

    so  the eColorFormat  is wrong  .

    omx_proxy_common.c        

    OMX_ERRORTYPE PROXY_AllocateBuffer(OMX_IN OMX_HANDLETYPE hComponent,
        OMX_INOUT OMX_BUFFERHEADERTYPE ** ppBufferHdr,
        OMX_IN OMX_U32 nPortIndex,
        OMX_IN OMX_PTR pAppPrivate, OMX_IN OMX_U32 nSizeBytes)

    if (nStride == LINUX_PAGE_SIZE && \
                pCompPrv->proxyPortBuffers[nPortIndex].proxyBufferType != EncoderMetadataPointers) //Allocate 2D buffer

    typedef enum PROXY_BUFFER_TYPE
        {
            VirtualPointers,   /*Used when buffer pointers come from the normal A9 virtual space */
            GrallocPointers,   /*Used when buffer pointers come from Gralloc allocations */
            IONPointers,       /*Used when buffer pointers come from ION allocations */
            EncoderMetadataPointers,        /*Used when buffer pointers come from Stagefright in camcorder usecase */
            BufferDescriptorVirtual2D          /*Virtual unpacked buffers passed via OMX_TI_BUFFERDESCRIPTOR_TYPE */
        } PROXY_BUFFER_TYPE;

    My   buffer  is not  from  stagefright , so  i think  proxyBufferType should be VirtualPointers. Is that right? if it is right  why  the judge above  have no effort?

    Further more,the result  264  file after the command   has not sps/pps, Is  the  state of omx_h264enc  right?even the colorformat  is wrang ,  the sps/pps  should in the 264 file.  

    Thank you very much!

  • Aaron,

    Encoders on OMAP4 supports  OMX_TI_COLOR_FormatYUV420PackedSemiPlanar as input format only. This format refers to the NV12 buffer holding Y an UV buffers in contiguous memory area. 

    Regards,

    Chintan

  • Aaron;

    I check the code and there is not clear why code is changing it to non TI index when it is passed Ducati side. I  imagine that if you use OMX_TI_COLOR_FormatYUV420PackedSemiPlanar your code works and it is not needed to use the other index or to specify it, can you confirm this observation?

    I have read the code for AFS and Video encode-decode code, they do some check up about this OMX_TI_COLOR_FormatYUV420PackedSemiPlanar value in some places before reaching the OMX_StateIdle state, that could be the reason why it is not taking affect the use of OMX_COLOR_FormatYUV420PackedSemiPlanar that is assigned to Port definitions structure afterwards.

    About

    if (nStride == LINUX_PAGE_SIZE && \
                pCompPrv->proxyPortBuffers[nPortIndex].proxyBufferType != EncoderMetadataPointers) //Allocate 2D buffer

    Can you check comments made in

    http://e2e.ti.com/support/omap/f/849/p/192468/691188.aspx

    this ti check if proper path is open for code selection.

    About buffer size, DOMX has specific buffer requirements then they are calculated internally and if needed some change it is communicated using port reconfiguration event.

    Two situation I know you could use to modify buffer size, is 1. if you plan to use a METADATA structure added to your buffer and 2. you need to reduce input buffer size for video encode, actual value is worst case scenario to use and to avoid reallocating buffers if input stream has a frame bigger than current size.

    About SPS+PPS you posted it in another post

    http://e2e.ti.com/support/omap/f/849/p/193242/691276.aspx

    But here are those answers:

    1. Can you do a buffer dump at OMX_FillBufferDone to check if SPS+PPS are being send from video encoder, you can dump only first 32 bytes that must be enough to see SPS+PPS and initial headers for first IFrame. This to discard failed areas or isolate the issue to one area.

    2. If you are using a full pipe line to encode-decode process and then to a check, if encoder is generating the SPS+PPS they are stored in GST decoder in a variable like codec data, for what I know, I don't have much data about your actual GST, it is required to read this variable when decoding process is started and send it before sending the first Iframe.

    It is needed to check full configuration and possibly to check some logs for something that could be wrong before these unsuccessful calls.

    if (nStride == LINUX_PAGE_SIZE && \
                pCompPrv->proxyPortBuffers[nPortIndex].proxyBufferType != EncoderMetadataPointers) //Allocate 2D buffer

  • Hi!

         I  dump the buffer at OMX_FillBufferDone  and   find  the sps+pps in the 264 file produced by ics. I have run the command on the android 2.3 and omap4 .the 264  file produced  by 2.3 contain sps+pps .the  sequence  is 00  00  00  01 27  and  00  00  00  01  28  .the gst-openmax source code on ics 4.0.3 has gotten   from the android 2.3.  The 264 file produce by ics  do not have the sps+pps  at the beginning  of the file  ,  at  that location  is  00  00  00  01  25   this is IDR.   If  i use the gstreamer filesrc the  output  port  proxyBufferType is VirtualPointers. so the omx_h264enc  can run on the ics 4.0.3 and  omap4 . but  the content of pictures which  of  video file produced by encoder are error.for example , two neighbouring  frames has encoded into one picture or  the chroma in the pictures are wrong .but the first picture is right ,both luminance and chroma.so I think  if the color format is wrong,the Y will be right but the UV must be wrong in all of picture.i think  this phenomenon is about the synchronization . is it right? what  configuration will influence the omx_h264enc  produced sps+pps?

    Thank you!

  • You can check next file for OMX_VIDEO_PARAM_AVCNALUCONTROLTYPE

    ./4ai/4AI.1.1/mydroid/hardware/ti/domx/omx_core/inc/OMX_TI_Video.h

    It needs to be set when OMX_StateLoaded with OMX_SetParameter.

    Read .h file for more details about it's use.

    About incomplete pictures, try to check input buffer contents.

  • In my previous post I referenced code to 4AI1.1 but it is present actually in latest 4AI1.5 too. Please refer to 4AI1.5 code instead.

  • Hi,

        now the luminance and chrome of 264  file  are all right.  because  i  expand  the width of input yuv buffer  in the videoparse plugin  to 4096 but  not notice the offset ,  so  the picture  are wrong.the color format is OMX_COLOR_FormatYUV420PackedSemiPlanar.

       Thank you very much !

       Br,

     yangliming