This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

New HeapMem Instance disappear from HeapMem tree in SYS/BIOS

I'm migrating from DSP/BIOS to SYS/BIOS and am using the *.cfg file in SYS/BIOS to create a HeapMem instance. When I right-click on HeapMem (in the Outline window), and choose New HeapMem..., CCSv5.1.1 will momentarily create a new heapmem which will display under the HeapMem tree briefly then disappear. Even on the HeapMem tab for the *.cfg file, after clicking on the Instance button (under the Variable Size Heap Management - Instance Settings heading) then clicking on the Add...button, the new heapmem will momentarily display in the Outline window under the HeapMem tree then disappear. Because the heapmem instance disappears, I can't configure it.

Why is the new heapmem instance disappearing from view?