This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

turning on debugging in linux kernel source

Hi,

I have an am-1808 (evm zoom kit). and i am developing a driver for am-1808. I need to view the log messages of the kernel source,

My code calls a method davinci_cfg_reg(const unsigned long index) defined in linux/arch/arm/plat-omap/mux.c, now in the end of this method there are few messages

if (warn) {
#ifdef CONFIG_DAVINCI_MUX_WARNINGS
        printk(KERN_WARNING "MUX: initialized %s\n", cfg->name);
#endif
    }

#ifdef CONFIG_DAVINCI_MUX_DEBUG
    if (cfg->debug || warn) {
        printk(KERN_WARNING "MUX: Setting register %s\n", cfg->name);
        printk(KERN_WARNING "       %s (0x%08x) = 0x%08x -> 0x%08x\n",
               cfg->mux_reg_name, cfg->mux_reg, reg_orig, reg);
    }
#endif

i want to view the values of cfg->mux_reg_name and other parameters, how can i do that ?

do i need to enable CONFIG_DAVINCI_MUX_DEBUG=y, CONFIG_DAVINCI_MUX_WARNINGS=y in the .config file ?

and if i do so, would need to replace the kernel of my board ?

and is there any other way i can see these log messages without changing the kernel ?

And these messages will be viewable by "dmesg" command ?

Thanks in advance

regards

usama