This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 1080P@30fps decode net stream Issue

Here we want to use dm368 to decode 1080P@30fps H.264 network stream,which is from network in MPEG2-TS format. But after doing some effort,we found that DM368 seemed to can only decode from .264 file,but not from network stream.When H.264 stream with bitrate @8Mbps, error normaly happen,expecially when IDR frame comes.Seems like decode DEMO escaped 80%~90% of cpu time.

I want to ask is there any one who use Here we want to use dm368 to decode 1080P@30fps H.264 network stream successfully, and how much cpu time used in decode&stream handle.

Thanks