This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omap L138 TRM: Suspected typo in SPIBUF.RXEMPTY

Hi,
In table 30-22 SPI Buffer Register (SPIBUF) Field Descriptions of L138 TRM SPRUH77, SPIBUF.RXEMPTY field is said to SET when either

·         Hosts reads the SPIBUF field (“the SPIBUF field” should refer to RXEMPTY field)

·         Host reads the whole SPIBUF register

It doesn’t seem to make sense because RXEMPTY basically is an indication bit, and it should not change value (including set) when host reads it. I suspect it might be a typo and the correct text should be “When host reads the SPIBUF RXDATA field”?
 
Paul