This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Omap4460:Crashed when setting IndexConfigVideoAVCIntraPeriod Dynamically.

Hi all,

Omap4460 & android4.0:

My demo will  crash When setConfig OMX_IndexConfigVideoAVCIntraPeriod .

OMX_IndexConfigVideoAVCIntraPeriod can be set Dynamically? Or I can only set it at Initialization time.

regards,

changwenliang

  • Hi Chanwenliang,

    In general, all the OMX_IndexConfig* can be set dynamically in run time. But this config parameter "OMX_IndexConfigVideoAVCIntraPeriod " is an exception which can set only when OMX Component is in loaded state. Since this AVCIntraPeriod structure contains nIDRPeriod which can be set to the codec at the initialization time.

    Thanks & Best Regards,

    Venkat