This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does SD Card Boot and Flashing Tool support 8G SD Card?

I  use a 8G SD card to boot DM365 board, but it stops after print such information like below

SD card boot and flashing tool for DM355 and DM365
by Constantine Shulyupin  http://www.LinuxDriver.co.il/
Online manual: http://wiki.davincidsp.com/index.php/SD_card_boot_and_flashing_tool_for_DM355_and_DM365
based on TI DM35x FlashAndBootUtils? 1.10 SFT, TI flash_utils and SpectrumDigital? evmdm355, evmdm365
Compiled on May 9 2012 at 18:29:27 with gcc 4.2.0 (MontaVista? 4.2.0-16.0.32.0801914 2008-08-30)
SYSTEM->DEVICE_ID=0x8B83E02F
&EMIFStart=0x02000000
nand->devID=0x000000F1 nand->dataBytesPerPage=2048 nand->pagesPerBlock=64 nand->numBlocks=1024 nand_size=134217728
sdcard_init

I have anther 2G SD card,it can work normally.

Does SD Card Boot and Flashing Tool support 8G SD Card?

What is the difference between 2G and 8G SD Card?

Thank you.