This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1810 Jlink Script

Other Parts Discussed in Thread: AM1808, AM1810, PROFIBUS

I am using a MCU AM1808 and it works fine.
Now I try to program a AM1810 by using the same hardware and software (low level SW, some GPIO-tests, etc).
Unfortunately I cannot manage the SW download via JTAG to the AM1810 although the AM1810 JTAG ID can be read correctly. The same SW and HW is running properly on a AM1808 target device. Unfortunately I have only the JLink Script File for the AM1808 although AM1810 and 1808 should be compatible.

Has anybody made some experiences concerning the AM1810 and IAR Embedded Workbench for ARM? Has anybody already managed to download some SW on the controller using IAR Embedded Workbench for ARM?

Kind regrads
Matt

  • Matt:

    I plan to take this up with IAR and Segger to see if we can get it resolved. Vincent Dubey contacted my about this issue. I want to double check on a few points:

    1. My  understanding is that that you are not using the EVMs but have made your own custom board. The custom board wiht the AM1808 works fine but the version with the AM1810 does not. Is this correct or are you using the EVMs?

    2. If you have your own custom board, would you be willing to provide one to Segger and/or IAR to help resolve the problem?

    3. Can you list which versions of IAR EWARM and J-Link you are using.

    Thanks, Nick

  • Hi Nick

    1. We are using our custom board which is made for the AM1808 AND the AM1810 (assembly variant). First we developed the firmware for the AM1808 which works fine. Now we develop the firmware for the AM1810 (Profibus DP) on the same hardware board (assembled with the AM1810).
    Unfortunately I cannot manage to download the firmware via JTAG (IAR and JLINK) to the AM1810. We don't use the EVM.

    2. Yes, we are willing to provide Segger and/or IAR with our custom hardware.

    3. I am using IAR EWB version 6.30 (also tried version 6.10) and J-Link version 4.50a

    Please contact me via Email (Mr. Dubey can give it to you) for further discussions.

    Thank's a lot!

    Regards Matt