This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Audio Capacitve Touch BoosterPack 430BOOST-C55AUDIO1 Initialisation Problem



My C5000 ACDP Booster Pack does not start up as described in the Quick start guide.

Functional Description:

After USB power up the red leds on the capacitive touch board flash clock and counter clockwise and turn off afterwards. The OLED Display remains dead all the time.

After 30 seconds all red leds turn on and flash simultaneously for approx. 5 seconds After that, the whole sequence repeats indefinitely. Concurrently the connected PC (Windows XP) recognizes a new hardware TCSC5505 and cannot find the corresponding driver software.

Hardware Lot No: HD1203011

Thomas Weber

  • Hi Thomas,

    It sounds like the DSP is not booting from the SD card...

    Normally the green XF LED (left of the OLED) turns on before then off after booting...

    If always on... Is the SD card correctly inserted into the BoosterPack board?

    If never on... Is power supplied to the BoosterPack (Jumper JP3 populated), USB connector on boosterpack used?

    What are your launchpad / boosterpack jumper settings?

    See also the ACTBP wiki pages: http://processors.wiki.ti.com/index.php/ACTBP

    Regards,
    Mark