Other Parts Discussed in Thread: ADS1256
Hi Community!
I'm stuck with a big problem:
For mi Bachelor Thesis I want to connect an ADS1256 to a 6713DSK and do some filtering..
If've done all the hardware stuff und now I'm trying to get the communication to the ADS working.
I have seen an example from TI (4705.ADS1256-C6713-CCS3v1), which in fact does exactly what I want. But I cant explan how this example should work.
The main problem is:
How can a McBSP be used to comunicate in SPI style?
I can send data whit McBSP_write. I can read back data with McBSP_read.
But when I want to read out a register or data from the ADS I need to do both operations in one CS sequence! Doing a write operation and a read operation will produce 2 CS sequences! This does obviously not work with an SPI device like the ADS1256.
So could someone please explain me, how this is done? See the exampe code for reading a register:
static unsigned int ReadRegister(TADS1256 *pADS,unsigned int uiRegister)
{
unsigned int iReadValue;
/* change the McBSP mode to 16 bits */
(void)SetWordLength(pADS->serial->hMcbsp,
ADS1256_WORDLENGTH_16BIT);
(void)SendCommand(pADS->serial->hMcbsp,
uiRegister | ADS1256_CMD_RREG);
/* change the McBSP mode to 8 bits */
(void)SetWordLength(pADS->serial->hMcbsp,
ADS1256_WORDLENGTH_8BIT);
/* wait the necessary number of cycles */
(void)Wait(pADS, 60);
/* send a dummy word to trigger 8 SCLKs */
while (MCBSP_FGETH(pADS->serial->hMcbsp, SPCR, XRDY) != 1) ;
MCBSP_write(pADS->serial->hMcbsp, 0);
/* and get the data */
while (MCBSP_FGETH(pADS->serial->hMcbsp, SPCR, RRDY) != 1) ;
iReadValue = MCBSP_read(pADS->serial->hMcbsp) & 0x000000FFu;
return iReadValue;
}
Is there additional hardware used in this project, which makes one CS frame out of two or how is this working?
Im trieing to get this to work for 2 days now.. :(
Thanks for any help!