Other Parts Discussed in Thread: AM3359, TMDXEVM3358
Hi,
We are working on the AM3359 IDK.
U-boot and the linux kernel are compiled like explained on wikis(http://processors.wiki.ti.com/index.php/Sitara_Linux_Software_Developer%E2%80%99s_Guide), with am335x-evm-sdk-src-05.04.01.00.tar.gz .
We create the SD card with the create-sdcard.sh script.
There are two partitions: the first one is boot, with MLO, u-boot.img and uImage files
The second one is rootfs, empty.
The SW3 and SW4 switches are configure for a SD boot.
When we switch-on the card, the Minicom window displays:
"Uncompressing Linux... done, booting the kernel"
Ok, but we don't have the u-boot shell. Do you know how to do?
Thanks a lot.
GF.