This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MessageQ example error on C6A816x

Hi,

I am using ti-ezsdk_dm816x-evm_5_03_01_15 software(unpacked with Ubuntu 10.04 LTS) on CentOS 5.8 with CodeSourcery toolchain. I was able to build syslink examples like messageQ. But I have trouble running it on either a C6A8167 custom board or a SD 816x EVM DDR 2 version board. Following is the error messages I got. Can someone please point out what went wrong with my setup?

Thanks,

Zhao

root@WCS:~# ./messageqapp_debug 1 DSP ./messageq_ti81xx_dsp.xe674
MessageQApp sample application
OsalDrv driver open: /dev/syslinkipc_Osal: No such file or directory
OsalDrv driver close: /dev/syslinkipc_Osal: Bad file descriptor
/dev/syslinkipc_MultiProc: No such file or directory
MultiProc driver close: : Bad file descriptor
SharedRegion driver open: : No such file or directory
SharedRegion driver close: : Bad file descriptor
/dev/syslinkipc_GateMP: No such file or directory
/dev/syslinkipc_MessageQ: No such file or directory
MessageQ driver close: : Bad file descriptor
Notify driver open: /dev/syslinkipc_Notify: No such file or directory
Notify driver close: /dev/syslinkipc_Notify: Bad file descriptor
ProcMgr driver open: /dev/syslinkipc_ProcMgr: No such file or directory
ProcMgr driver close: /dev/syslinkipc_ProcMgr: Bad file descriptor
/dev/syslinkipc_HeapBufMP: No such file or directory
/dev/syslinkipc_HeapMemMP: No such file or directory
/dev/syslinkipc_ListMP: No such file or directory
/dev/syslinkipc_RingIO: No such file or directory
RingIO driver close: : Bad file descriptor
/dev/syslinkipc_RingIOShm: No such file or directory
RingIO driver close: : Bad file descriptor
/dev/syslinkipc_ClientNotifyMgr: No such file or directory
ClientNotifyMgr driver close: : Bad file descriptor
/dev/syslinkipc_FrameQBufMgr: No such file or directory
FrameQBufMgr driver close: : Bad file descriptor
/dev/syslinkipc_FrameQ: No such file or directory
FrameQ driver close: : Bad file descriptor
/dev/syslinkipc_Ipc: No such file or directory
Assertion at Line no: 349 in /home/zhaoli/ti-ezsdk_dm816x-evm_5_03_01_15/component-sources/syslink_2_00_05_85/pacd
Assertion at Line no: 349 in /home/zhaoli/ti-ezsdk_dm816x-evm_5_03_01_15/component-sources/syslink_2_00_05_85/pacd
Assertion at Line no: 349 in /home/zhaoli/ti-ezsdk_dm816x-evm_5_03_01_15/component-sources/syslink_2_00_05_85/pacd
Invalid <Core name> specified!
Usage : ./messageqapp_<debug|release> <Number of slave cores> <Core name 1> <File path 1> <Core name 2> <File pat.

Supported core names: