This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 Infrared

Hi,

We have the DM8127J3 camera with Aptina 10M MT9J003 CMOS sensor, can we re-configure it with another CMOS sensor with the following specifications?

2MB+

IR 750um+(not near IR)

Thanks.

  • Hi, 

    The ipnc_rdk supports upto 10M resolutions demo, so certainly a higher resolution than default is supported.

    We haven't validated any IR sensor, but if you can get the raw capture data from Video port into DDR is that sufficient? Also interface protocol is used by the IR sensor?

    Regards

    Rajat