This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dynamic Library Not Found - EZDSP5355 - Learning CD Chapter 1

Hi,

I am experiencing a problem running chapter 1 of the learning CD when using the EZDSP5355. Noting that I'm on chapter 1, it is clear I'm not well equipped to solve this on my own :(

The problem is that:

XDS100V2 USB Em...

Error connecting to the target:
(Error -600 @ 0x0)
A required dynamic library could not be located.
The library isn't on the search path.
(Release 5.0.429.0)

I followed the directions found here:

Here is the console output:

http://e2e.ti.com/support/dsp/tms320c5000_power-efficient_dsps/f/109/t/140749.aspx

With the exception that rather than editing files by hand I copied in the suite of four files that differ from the 5535.

Help getting off square one would be very appreciated.


**** Build of configuration Debug for project FirstProject-SecondTry ****

C:\Program Files (x86)\Texas Instruments\ccsv4\utils\gmake\gmake -k all
'Building file: ../PLL.c'
'Invoking: Compiler'
"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5515 -g --include_path="C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/include" --diag_warning=225 --ptrdiff_size=32 --memory_model=huge --preproc_with_compile --preproc_dependency="PLL.pp" "../PLL.c"
'Finished building: ../PLL.c'
' '
'Building file: ../aic3204.c'
'Invoking: Compiler'
"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5515 -g --include_path="C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/include" --diag_warning=225 --ptrdiff_size=32 --memory_model=huge --preproc_with_compile --preproc_dependency="aic3204.pp" "../aic3204.c"
'Finished building: ../aic3204.c'
' '
'Building file: ../aic3204_init.c'
'Invoking: Compiler'
"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5515 -g --include_path="C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/include" --diag_warning=225 --ptrdiff_size=32 --memory_model=huge --preproc_with_compile --preproc_dependency="aic3204_init.pp" "../aic3204_init.c"
'Finished building: ../aic3204_init.c'
' '
'Building file: ../main.c'
'Invoking: Compiler'
"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5515 -g --include_path="C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/include" --diag_warning=225 --ptrdiff_size=32 --memory_model=huge --preproc_with_compile --preproc_dependency="main.pp" "../main.c"
'Finished building: ../main.c'
' '
'Building file: ../stereo.c'
'Invoking: Compiler'
"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5515 -g --include_path="C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/include" --diag_warning=225 --ptrdiff_size=32 --memory_model=huge --preproc_with_compile --preproc_dependency="stereo.pp" "../stereo.c"
'Finished building: ../stereo.c'
' '
'Building file: ../usbstk5505.c'
'Invoking: Compiler'
"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5515 -g --include_path="C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/include" --diag_warning=225 --ptrdiff_size=32 --memory_model=huge --preproc_with_compile --preproc_dependency="usbstk5505.pp" "../usbstk5505.c"
'Finished building: ../usbstk5505.c'
' '
'Building file: ../usbstk5505_gpio.c'
'Invoking: Compiler'
"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5515 -g --include_path="C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/include" --diag_warning=225 --ptrdiff_size=32 --memory_model=huge --preproc_with_compile --preproc_dependency="usbstk5505_gpio.pp" "../usbstk5505_gpio.c"
'Finished building: ../usbstk5505_gpio.c'
' '
'Building file: ../usbstk5505_i2c.c'
'Invoking: Compiler'
"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5515 -g --include_path="C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/include" --diag_warning=225 --ptrdiff_size=32 --memory_model=huge --preproc_with_compile --preproc_dependency="usbstk5505_i2c.pp" "../usbstk5505_i2c.c"
'Finished building: ../usbstk5505_i2c.c'
' '
'Building file: ../usbstk5505_led.c'
'Invoking: Compiler'
"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5515 -g --include_path="C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/include" --diag_warning=225 --ptrdiff_size=32 --memory_model=huge --preproc_with_compile --preproc_dependency="usbstk5505_led.pp" "../usbstk5505_led.c"
'Finished building: ../usbstk5505_led.c'
' '
'Building target: FirstProject-SecondTry.out'
'Invoking: Linker'
"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5515 -g --diag_warning=225 --ptrdiff_size=32 --memory_model=huge -z -m"FirstProject-SecondTry.map" --warn_sections -i"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/lib" -i"C:/Program Files (x86)/Texas Instruments/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/include" --reread_libs --rom_model -o "FirstProject-SecondTry.out" "./usbstk5505_led.obj" "./usbstk5505_i2c.obj" "./usbstk5505_gpio.obj" "./usbstk5505.obj" "./stereo.obj" "./main.obj" "./aic3204_init.obj" "./aic3204.obj" "./PLL.obj" -l"libc.a" "../55xdsph.lib" "../CSLc55x5h.lib" "../lnkx.cmd"
<Linking>
'Finished building target: FirstProject-SecondTry.out'
' '
Build complete for project FirstProject-SecondTry