I am attempting to get the ECU module in the VoLIB to work on TMS320C6A8168 processor.
It seems to be working - with the exception that the echo canceller is not cancelling the echo.
I can not understand the following meaning:
"In addition to the guidelines in the above table, buffers 2, 5, 6 and 14 should not be in the same bank as the object code eculms.obj (.text). Additionally, buffers 2 and 5 should not be in the same bank as ecuerm.obj (.text)."
I do not know how to set up different bank.
Any other suggestions for things to check or mistakes I am making would be greatly appreciated.