This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building problem on helloDSP wiki project



Hello everybody.Now I am working on the SEED OMAPL137 evm board. 

I downloaded the "Example application using DSP Link on OMAPL1x (TI  wiki)" related docunments and tried to build the project in Linux

I changed BASE_TOOLCHAIN, DSPLINK etc according to my installation and DSPLINK version.

The DSP side building is correct, however, the GPP side is not built:

[root@David helloDSPgpp_1_10]# make

make: execvp: /opt/montavista/pro/devkit/arm/v5t_le:      permission denied

make:*** [Debug/helloDSP.o] ERROR 127

The GPP side makefile is "rwx" and BASE_TOOL_CHAIN, CC, DSPLINK are correct. Also arm_v5t_le-gcc is correct when build other projects.

So how to solve this problem? 

  • I used the CodeSourcery toolchain on my project but I had no problems building helloDSP using the Montavista toolchain. Here's my settings in Makefile:

    BASE_TOOLCHAIN := /opt/mv_pro_5.0/montavista/pro/devkit/arm/v5t_le
    CC := arm_v5t_le-gcc
    DSPLINK := /opt/OMAPL137_arm_1_00_00_11/dsplink-1_61_03-prebuilt/packages/dsplink

    Your paths will be different. May check the permissions on the directory

    /opt/montavista/pro/devkit/arm/v5t_le

  • Thanks.

    I used the Montavista toolchain and the permissions on the /opt/montavista/pro/devkit/arm/v5t_le is correct. There is no error when using arm_v5t_le-gcc to build other codes .