I want to try the USB-IF compliance test for our custom board using AM3505 and Linux.
Following LinuxPSP is used.
http://software-dl.ti.com/dsps/dsps_public_sw/psp/LinuxPSP/OMAP_04_02/04_02_00_07/index_FDS.html
Following driver is used for USB0(OTG).
/linux-04.02.00.07/drivers/usb/musb/am35x.c
Following driver is used for HSUSB0.
/linux-04.02.00.07/drivers/usb/host/ehci-omap.c
Is the USB-IF compliance test supported by these drivers?
If it is not supported, what should I do to try the USB-IF compliance test?
Best regards,
Daisuke