This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Omap 4460:The Decoder output data has mosaics.

Hi all,

Using Hardware H264 decoder, the output data has mosaics while the input bitstream doesn't.

And it doesn't happen when using sofware decoder.

Can it turn better through setting any decoder params or configs?

Bitstream: Base profile 640*480  10fps 512kbps

Based on android 4.0.3

Below params have already set:

OMX_IndexParamVideoPortFormat  OMX_IndexParamPortDefinition(Input/output)