This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Basic Questions: Overall picture of captured data streaming on DM8168

I am trying to understand architecture of VPSS related to HDVICPs for DM8168. I don't have much firmware background.

What I managed to do so far is to load load-hd-v4l2-firmware.sh on my DM8168-EVM, and managed to capture 1080p60 video through Y Pr Pb ports on daughter board and encode it to a file, using Gstreamer pipeline code:

gst-launch v4l2src always-copy=false queue-size=12 num-buffers=2000 ! 'video/x-raw-yuv-strided,format=(fourcc)NV12,width=1920,height=1080,framerate=(fraction)60/1' ! omxbufferalloc numBuffers=12 ! omx_h264enc bitrate=5000000 ! gstperf ! filesink location=v4l2cap.h264

But I want to know how many HDVICPs are actively encoding when I used the above Gstreamer pipeline. So I start looking at the Figure1 and Figure2 to understand system architecture of the DM8168.

.


Q1. I can see there are several video pipelines and graphic pipelines in Figure1. What does this pipeline exactly mean? (Is this a software path for data stream to pass through?) And what is the difference between Video and Graphic pipeline?

Q2. Does one of these graphic or video pipelines have something to do with capturing driver? If I type the above Gstreamer command, I know the video image is coming in through v4l2 driver. But which pipeline does this captured video stream go?

Q3. Once the video stream passes one of pipelines, the video stream should be encoded with H.264 codec to be stored in a file. But in Figure1, I only see four Encoder blocks right before some kind of output ports?(DVO0, HDComp, SD) I think basically I want to know where my captured video stream goes through on Figure1.

Q4. Where does HDVICP coprocessor actually do the work? From my shallow understanding, I think it should be helping the encoder blocks. Is this correct? If only one Encoder block is used, is only one HDVICP doing the encoding?
.


Sorry for asking many questions. But I have gone through all the user guides(VPSS , video driver guides, SDGuide, etc...) to understand overall pictures, but the guides seem assume readers have some background in embeded system and firmware which I don't. Any your replies would be much appreciatd.

Figure1

Figure2

  • The figures you have shown are not the complete system - they are only the display part of the VPSS which in fact you are not using for your application.

    There are three major components:

    • capture component of VPSS - this handles the v4l2src part of pipeline
    • HD-VICP - this is the actual video encoder/decoder blocks that in your case are doing H264 encoder
    • display component of VPSS - this handles the scalars, deinterlacer, grpahics plane blending and driving of the output ports hdmi/dvi  etc. It is not used in your case.