This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hyplnk_readRegs runs in infinite loop



Hi,

I'm trying to configure the hyperlink module for a communication between two C6678 and I'm having some issues when I try to read the registers of the remote DSP.

After initialization, I check this registers:

hyplnkStatusReg_s::link = 1

hyplnkStatusReg_s::serialHalt = 0

hyplnkStatusReg_s::pllUnlock = 0

This normaly means that the hyperlink module is up and I can normaly read the remote DSP registers.

But when I call this function:

Hyplnk_readRegs(hyplnk_handle,hyplnk_LOCATION_REMOTE,&getRegs);

it seems to run in an infinite loop...

When I change the destination to hyplnk_LOCATION_LOCAL it works fine so maybe it's a problem with the configuration part. But what I don't understand it's why the hyplnkStatusReg_s::link is set if the link is not working?

Anybody have an idea to resolve the problem ?