This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Appro DM365 SDK and PSIA support



Hello there,

Recieved from Appro SDK for DM365. It has commented out PSIA code.

For example, cam on GET /PSIA/Streaming/channels/

capabilities
answer 404, but there are this function in
ipnc_app/network/boa-0.94.13/src/psia_root.c:

void add_std_resources(node_t *parent, void *fn_index, void *fn_indexr,
void *fn_description, void *fn_capabilities)
{
 node_t *node;

.....

 if(fn_capabilities) {
   node = add_node(parent, "/capabilites", M_GET, NODE_STD, "1.0",
fn_capabilities);
   desc_get_function(node, "Return capabilities of the current resource");
   desc_get_result(node, "resource specific");
   desc_get_notes(node, "Returns a capabilities description of the
resource");
 }
}

And instead of using this it was commented:

static int root_build_tree(node_t *parent)
{
 node_t *node;

 node = add_node(parent, "/System", M_NULL, NODE_SERVICE, "1.0",
&process_system);
 desc_get_function(node, "System service");
 //add_std_resources(node, &process_index, &process_indexr,
&process_description, NULL);

 node = add_node(parent, "/Security", M_NULL, NODE_SERVICE, "1.0",
&process_security);
 desc_get_function(node, "Security service");
 //add_std_resources(node, &process_index, &process_indexr,
&process_description, NULL);

 node = add_node(parent, "/Streaming", M_NULL, NODE_SERVICE, "1.0",
&process_streaming);
 desc_get_function(node, "Streaming service");
 //add_std_resources(node, &process_index, &process_indexr,
&process_description, NULL);

 return (build_tree_error());
}

Appro techsupport engineer told thats was made by TI:

> The part of PSIA function was edited by TI's engineer. Please ask TI E2E
> Community or contact with TI directly to get more information about PSIA.
> Thanks.

Why?

Best regards, Andrei "MEZON" Shvetsoff

Devline Testing Engineer