Other Parts Discussed in Thread: OMAPL138
hello:
I am using c6747, now I want to burn the spi flash by the uart, and I don't know how to do it? Can anyone give me some advice? Example is the best!
Thanks very much!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Si,
In order to burn flash on the device for boot using UART, TI provides a flash and boot utility called serial flash utility. This is part of the boot and flash utilities that can be downloaded here:
http://sourceforge.net/projects/dvflashutils/files/OMAP-L137/
In order to create a boot image you need to convert you application out file to an AIS boot file using the AIS Gen tool. The process of doing this and flashing the device has been described with an LED blinking example on the following wiki:
http://processors.wiki.ti.com/index.php/Boot_Images_for_OMAP-L137
Hope this answers your question. Good luck!!.
Regards,
Rahul
thanks for your reply!
1. Is it useful to c6748 too? I want to use this tool to burn c6748 by the uart port!
2. I had install the AISgen for D800K008,. and it has uart boot host tool, it can be used to burn the spi flash by the uart port? and what should i do?
thanks very much!
Si,
The links that I posted on my earlier reponse were specific to OMAPL137/C6747 devices.
If you are using C6748 devices you have downloaded the correct AISGen package. For boot examples and links to tools and utilities on C6748 refer to this wiki:
http://processors.wiki.ti.com/index.php/Boot_Images_for_OMAP-L138
Please ensure you use the correct ROM ID while creating your image. All details of finding the ROM ID on your device is described in the boot loader app Note for OMAPL138. You should also find this wiki useful to understand the boot process on C6748
http://processors.wiki.ti.com/index.php/OMAP-L138_Bootloader
Regards,
Rahul
Rahul,
I had read your links, and it doesn't give me advise to burn spi flash, so now I am still puzzled about how to burn the spi flash !
can you tell me the steps about how to burn the spi flash? Best, give me some pictures step by step to show how to operate !
Thanks very much!
Regards,
Si
Si,
I strongly recommend following the instructions on that wiki rather than just reading the wiki. This is a very simple example and should take more than 15 min of your time. If you download the example package distributed on the Boot images wiki, there is a precompiled SPI flash boot image in it. When you follow the instructions instructions, the wiki provides links to the serial flash wiki that describes flashing SPI flash:
For OMAPL137/C6747:
http://processors.wiki.ti.com/index.php/Serial_Boot_and_Flash_Loading_Utility_for_OMAP-L137
For OMAPL138/C6748:
http://processors.wiki.ti.com/index.php/Serial_Boot_and_Flash_Loading_Utility_for_OMAP-L138.
These wikis provide all the boot switch options as well as the options that can be used with sfh tool that may be required.
Regards,
Rahul