I am newer to video system design. From 8168 ds, there are three HDVICP2, each can do a single 1080P60 H.264 encode or decode. I am not clear about video input ports. There are two VIP: VIP0 and VIP1. VIP0 is 24bit, and VIP1 is 16bit, and each VIP can be configured as two 8-bit ports.
1. Does it mean 8168 only can accept up to 4-ch video input if only using VIP?
2. If it is configured as 8-bit port, can it capture 1080P60 HD video?
By the way, 8168 has C674x DSP, what about its capability? Can it also handle one channnel 1080P60 H2.64 encode or decode?
Thanks
Peter