hi,
when i used DM8168 HDVICP to encode/decode 1080p60fps, there was a warning coming out. the targetfps is 30. i'm using RDK2.0.
Does someone face the same question? thanks for help! :)
-------------------------------------------------------------------------
"[m3video] Channel:0 inputframerate:60 targetfps:30"
i setup the inputframerate as below:
--------------------------------------------------------
for (i=0; i<1; i++) {
encPrm.chCreateParams[i].format = chainsCfg->encFormat;
encPrm.chCreateParams[i].profile = chainsCfg->encProfile;
encPrm.chCreateParams[i].dataLayout = IVIDEO_FIELD_SEPARATED;
encPrm.chCreateParams[i].fieldMergeEncodeEnable = FALSE;
encPrm.chCreateParams[i].defaultDynamicParams.intraFrameInterval = 60;
encPrm.chCreateParams[i].encodingPreset = XDM_DEFAULT;
encPrm.chCreateParams[i].enableAnalyticinfo = 0;
encPrm.chCreateParams[i].rateControlPreset =
IVIDEO_LOW_DELAY;
encPrm.chCreateParams[i].defaultDynamicParams.inputFrameRate = 60;
encPrm.chCreateParams[i].defaultDynamicParams.targetBitRate =
gChains_networkCtrl.bitRate;
encPrm.chCreateParams[i].defaultDynamicParams.interFrameInterval = 1;
encPrm.chCreateParams[i].defaultDynamicParams.mvAccuracy =
IVIDENC2_MOTIONVECTOR_QUARTERPEL;
}
-------------------------------------------------------------------------