Other Parts Discussed in Thread: SYSBIOS
Hi,
I try to make project for syslink samples in ccs accordingly to this article (http://processors.wiki.ti.com/index.php/Creating_CCS_Project_for_SysLink_samples). Now i can build messageQ sample for dsp. But i cannot run it.
I use the same sysbios, ipc, syslink, xdctools as in ezsdk 5.04.00.11. I didn't rebuild linux side executable. Here is the trace output.
root@dm814x-evm:/usr/share/ti/syslink-examples/TI814X/messageq# ./slaveloader_debug startup DSP ./messageQ_DSP.out
Attached to slave procId 0.
Loading procId 0.
Loaded file ./messageQ_DSP.out on slave procId 0.
Started slave procId 0.
root@dm814x-evm:/usr/share/ti/syslink-examples/TI814X/messageq# ./messageqapp_debug
MessageQApp sample application
Run for all supported proc IDs
Entered MessageQApp_startup
Warning! Unsupported procID specified for running the sample application! proc I
D: [1]
Warning! Unsupported procID specified for running the sample application! proc I
D: [2]
After Ipc_loadcallback:
status [0x0]
*** Platform_startCallback: Ipc_attach timeout
Error [0xffffffff] at Line no: 2828 in file /swcoe/sdk/cm/netra/arago-tm
p/work/dm814x-evm-none-linux-gnueabi/ti-syslink-2_10_03_20-r1j/syslink_2_10_03_2
0/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/family/hlos/knl/ti81xx/Platform.c
*** Ipc_control: Platform_startCallback failed!
Error [0xffffffff] at Line no: 852 in file /swcoe/sdk/cm/netra/arago-tmp
/work/dm814x-evm-none-linux-gnueabi/ti-syslink-2_10_03_20-r1j/syslink_2_10_03_20
/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Ipc.c
Assertion at Line no: 301 in /swcoe/sdk/cm/netra/arago-tmp/work/dm814x-evm-none-
linux-gnueabi/ti-syslink-2_10_03_20-r1j/syslink_2_10_03_20/packages/ti/syslink/u
tils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Linux/IpcDrv.c: (status >= 0) : failed
Error in Ipc_control Ipc_CONTROLCMD_STARTCALLBACK[0xffffffff]
Leaving MessageQApp_startup ffffffff
What can i have missed in configuration?
I use dm8148 evaluation module, 2x512MB DDR3, CCS version 5.1.1.00031 (on Windows), ezsdk 5.04.00.11, bios_6_33_02_31, ipc_1_24_02_27, xdctools_3_23_01_43, syslink_2_10_03_20.