Other Parts Discussed in Thread: AM3359, TLK110
Hi,
I'd like to have more information about performances in Ethercat implementation with ARM3359.
I noted that the PRUs are 200MHz RISC processors and I'd like to have comparison, if it's possible, with hardware Asic ET1100 of Beckhoff.
One of the information I'm interested about, is the time tMM (MII PORT to MII port delay) that is 335ns in worst case of data to be processed in ET1100 (page III-93 of the Et1100 Hardware Description databook)
Which is this time in ARM3359?
Thanks
Luca