The manuals make it clear that it is still possible to use the legacy method of NC_SystemOpen, CfgNew, CfgAddEntry, NC_NetStart, etc. But I am not sure how to tell CCSv5, XCONFIG, et al, that I really want to use the legacy method. I'm getting a generated call to SystemOpen and NetStart that conflicts with the one that I am attempting to use. I have included NDK and NSP in the RTSC, and NDK shows up in the Sys/Bios Global area, with only the Global Network settings checked.
Should I have excluded NDK from the RTSC configuration? Something else?