This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

hwclock: can't open '/dev/misc/rtc': No such file or directory



Hi,

I m using DM355 processor and kernel 2.6.32, nw  i m unable to access h/w RTC in my target board,

pl refer my bootup log.,

DM35x initialization passed!
TI UBL Version: 1.50
Booting Catalog Boot Loader
BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000019.
   DONE
Jumping to entry point at 0x81080000.


U-Boot 2009.03 (Jun 21 2010 - 15:13:07)

I2C:   ready
DRAM:  128 MB
NAND:  NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron NAND 512MiB 3,3V 8-bit)
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
No NAND device found!!!
512 MiB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 216MHz
DDR Clock :- 171MHz
Hit any key to stop autoboot:  0
dm9000 i/o: 0x4014000, id: 0x90000a46
DM9000: running in 16 bit mode
MAC: 00:00:70:ff:3e:4e
operating at 100M full duplex mode
TFTP from server 10.10.30.62; our IP address is 10.10.30.56
Filename 'uImage'.
Load address: 0x80700000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ####################
done
Bytes transferred = 2098192 (200410 hex)
## Booting kernel from Legacy Image at 80700000 ...
   Image Name:   Linux-2.6.32-rc2-davinci1-HHT_V3
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2098128 Bytes =  2 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux..........................................................................................................
Linux version 2.6.32-rc2-davinci1-HHT_V3.0 (root@titus-desktop) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #176 PRE2
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DM355 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci dm355 variant 0x0
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 29464
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=10.10.30.56 root=/dev/nfs nfsroot=10.10.30.62:/home/titus/Desktop0
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 116MB = 116MB total
Memory: 113052KB available (3860K code, 355K data, 204K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 107.31 BogoMIPS (lpj=536576)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 104 gpio irqs
NET: Registered protocol family 16
MUX: initialized INT_EDMA_CC
bio: create slab <bio-0> at 0
DM355 IPIPE intialized in Single Shot mode
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
vpss vpss: dm355_vpss vpss probed
vpss vpss: dm355_vpss vpss probe success
ch0 default output "LCD", mode "320x240"

 VPSS_CLKCTRL C4 = 145555

 VPSS_CLKCTRL C7 = 79

 SYS_VPSS_CLKCTL = 18
VPBE Encoder Initialized
Hi.............This is titus from kernel space
MUX: initialized VOUT_FIELD_G70
LogicPD encoder initialized
Switching to clocksource timer0_1
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc: USB Host mode controller at fec64000 using DMA, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
JFS: nTxBlock = 884, nTxLock = 7075
msgmni has been set to 221
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler anticipatory registered (default)
Console: switching to colour frame buffer device 40x30
davincifb davincifb.0: dm_osd0_fb: 320x240x16@0,0 with framebuffer size 2025KB
davincifb davincifb.0: dm_osd1_fb: 320x240x4@0,0 with framebuffer size 300KB
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A
console [ttyS0] enabled
serial8250.0: ttyS1 at MMIO 0x1c20400 (irq = 41) is a 16550A
serial8250.0: ttyS2 at MMIO 0x1e06000 (irq = 14) is a 16550A
brd: module loaded
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xdc (Micron NAND 512MiB 3,3V 8-bit)
Creating 5 MTD partitions on "davinci_nand.0":
0x000000000000-0x000000f00000 : "bootloader"
usb 1-1: new high speed USB device using musb_hdrc and address 2
0x000000f00000-0x000001000000 : "params"
0x000001000000-0x000001400000 : "kernel"
0x000001400000-0x000021400000 : "filesystem1"
mtd: partition "filesystem1" extends beyond the end of device "davinci_nand.0" -- size truncated to 0x1ec00000
0x000020000000-0x000020000000 : "filesystem2"
mtd: partition "filesystem2" is out of reach -- disabled
davinci_nand davinci_nand.0: controller rev. 2.3
spi_davinci spi_davinci.0: DaVinci SPI driver in EDMA mode
Using RX channel = 17 , TX channel = 16 and event queue = 1
at25 spi0.0: 8 KByte at25640a eeprom, pagesize 32
spi_davinci spi_davinci.0: Controller at 0xfec66000
PINMUX0 = 32597
PINMUX0 = 31573
enable_tft_completed.
Inserting SPI module
PINMUX0 = 31573
PINMUX0 = 31658
SPI2 SPI2FMT0 value =173320
tft_open exit
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
dm9000 Ethernet Driver, V1.31
usb 1-1: configuration #1 chosen from 1 choice
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 4 ports detected
eth0: dm9000a at c7906000,c790a002 IRQ 65 MAC: 00:00:70:ff:3e:4e (chip)
usbcore: registered new interface driver cdc_acm
cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters
usbcore: registered new interface driver usbserial
usbserial: USB Serial Driver core
USB Serial support registered for pl2303
usbcore: registered new interface driver pl2303
pl2303: Prolific PL2303 USB to serial adaptor driver
usbcore: registered new interface driver usbtest
i2c /dev entries driver
Linux video capture interface: v2.00
vpfe_init
vpfe-capture: Unable to get vpfe config
vpfe-capture: probe of vpfe-capture failed with error -2
vpfe_register_ccdc_device: DM355 CCDC
vpfe capture not initialized
dm355_ccdc: probe of dm355_ccdc failed with error -14
Trying to register davinci display video device.
layer=c61c0a00,layer->video_dev=c61c0b70
Trying to register davinci display video device.
layer=c61c0200,layer->video_dev=c61c0370
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v0.1.0)
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
davinci_mmc davinci_mmc.1: Using DMA, 4-bit mode
usbcore: registered new interface driver hiddev
usbcore: registered new interface driver usbhid
usbhid: v2.6:USB HID core driver
Advanced Linux Sound Architecture Driver Version 1.0.21.
XXXXX: init001:
No device for DAI tlv320aic3x
No device for DAI davinci-i2s
XXXXX: probe101:
AIC3X Audio Codec 0.2
XXXXX: probe102:
XXXXX: probe103:
XXXXX: probe104:
asoc: tlv320aic3x <-> davinci-i2s mapping ok
Failed to add route HPLOUT->Headphone Jack
ALSA device list:
  #0: DaVinci EVM (tlv320aic3x)
SPCR1=0x0
RCR1=0x0
XCR1=0x0
SRGR1=0x20000001
PCR1=0x0
DXR1=0x0
SPCR1=0x2000000
XCR1=0x140
PCR1=0xA00
SRGR1=0x101F0F07
SPCR1=0x2F30000
Resetting DAC....done
 Configuring Audio DAC
SPI0 SPIFMT0 value =173320
SPI0 dv_open exit
before spi open
after init disp
TCP cubic registered
NET: Registered protocol family 17
Clocks: disable unused vpss_master
Clocks: disable unused vpss_slave
Clocks: disable unused mjcp
Clocks: disable unused asp0
Clocks: disable unused spi1
Clocks: disable unused spi2
Clocks: disable unused pwm0
Clocks: disable unused pwm1
Clocks: disable unused pwm2
Clocks: disable unused pwm3
Clocks: disable unused timer1
Clocks: disable unused timer3
Clocks: disable unused rto
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
mmc0: host does not support reading read-only switch. assuming write-enable.
mmc0: new high speed SDHC card at address b688
mmcblk0: mmc0:b688 SU08G 7.40 GiB
 mmcblk0: p1
eth0: link down
eth0: link up, 100Mbps, full-duplex, lpa 0x45E1
IP-Config: Guessing netmask 255.0.0.0
IP-Config: Complete:
     device=eth0, addr=10.10.30.56, mask=255.0.0.0, gw=255.255.255.255,
     host=10.10.30.56, domain=, nis-domain=(none),
     bootserver=255.255.255.255, rootserver=10.10.30.62, rootpath=
Looking up port of RPC 100003/2 on 10.10.30.62
Looking up port of RPC 100005/1 on 10.10.30.62
VFS: Mounted root (nfs filesystem) on device 0:13.
Freeing init memory: 204K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
udev: starting version 141
udevd[474]: inotify_add_watch(3, (null), 10) failed: Bad address

udevd[474]: inotify_add_watch(3, (null), 10) failed: Bad address

udevd[474]: inotify_add_watch(3, (null), 10) failed: Bad address

Remounting root file system...
mount: mounting /dev/root on / failed: Invalid argument
mount: mounting /dev/root on / failed: Invalid argument
modprobe: FATAL: Could not load /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep: No such file or directory

modprobe: FATAL: Could not load /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep: No such file or directory

WARNING: Couldn't open directory /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0: No such file or directory
FATAL: Could not open /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep.temp for writing: No such file or directory
modprobe: FATAL: Could not load /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep: No such file or directory

modprobe: FATAL: Could not load /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep: No such file or directory

modprobe: FATAL: Could not load /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep: No such file or directory

modprobe: FATAL: Could not load /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep: No such file or directory

root: mount: mounting rootfs on / failed: No such file or directory
modprobe: FATAL: Could not load /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep: No such file or directory

root: mount: mounting devpts on /dev/pts failed: No such device
modprobe: FATAL: Could not load /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep: No such file or directory

modprobe: FATAL: Could not load /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep: No such file or directory

ALSA: Restoring mixer settings...
Setting up IP spoofing protection: rp_filter.
Configuring network interfaces... done.
Mon Jun 21 15:23:00 UTC 2010
INIT: Entering runlevel: 5
Starting telnet daemon.
modprobe: FATAL: Could not load /lib/modules/2.6.32-rc2-davinci1-HHT_V3.0/modules.dep: No such file or directory

Starting syslogd/klogd: done
Starting thttpd.

 _____                    _____           _         _   
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
              |___|                    |___|            

Arago Project http://arago-project.org dm355-evm ttyS0

Arago 2009.11 dm355-evm ttyS0

dm355-evm login: root
root@dm355-evm:~#

root@dm355-evm:~# hwclock -r
hwclock: can't open '/dev/misc/rtc': No such file or directory
root@dm355-evm:~#

  • Hi Stalin,

     Have you Designed base board using DM355 or are you using EVM kit with DM355. This may be because of  bad address of RTC IC you are using. Check in the path "arch/arm/mach-davinci/board-dm355-evm.c" in that I2C section.  Check for i2c_board info, for example if i you are using ds1307 and its connected on i2C3 then it should be defined accordingly   "I2C_BOARD_INFO("ds1307", 0x68)," 0x68 is the address for ds1307.

     

  • Its perfect,

    Actually I did this already,

    but unfortunately i mentioned wrong address in the board file.,

    thanx for ur quick response

    thanks to god ,come out from this issue , u too...............