Hi,
On my custom board , c6713 has SRAM on CE2 and a FPGA on CE0. I can easily read /write on the sram after setting the ce2 register with the read/write timings. But I am unable to read/write from the FPGA. ( FPGA is working as A Synchronous SRAM with Read Enable, Chip enable, Write Enable and Output enable pins)
Debugging shows that on Read request from DSP , FPGA goes into the reading mode. But the data get by DSP is always 0.
Any suggestions , how to configure emif to communicate with FPGA.
Regards,
Anwar Naseem