Hi,all
platform: EVM 3730
os:wince 6.0
BSP:BSP BSP_WINCE_ARM_A8 1.01.00.03
camere: OV5640
In my camera driver,I use the pipeline-"Sensor ==> CCDC ==> Resizer ==> memory ",when output sequence of the ov5640 is set to YUYV, Preview is normal,See figure 1.
Figure 1 YUYV
but I change the output sequence to UYVY ,Synchronously,I also modify camer driver for UYVY format. Preview is abnormal,See figure 2.
Figure 2
who can tell me why?, what do I need to do?