Hi,
Have a brief question with EDMA3 controller registers on L138.
OMAP L138 has EDAMCC0, which has two TC’s; and EDMACC1, which has 1 TC. However, the register description for CC (section 18.4.2 of SPRUH77, page 624) and TC (section 18.4.3 of SPRUH77, page 663) does seem to contain information on the base address of individual CC’s and TC’s. Therefore when modifying register contents I don’t know exactly which CC and TC I am changing.
Is it needed to differentiate between different CC’s and TC’s?
Paul