This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

White balance in dm368 IPIPE driver



Hello!

I've used Adobe Lightroom together with XRite Passport plugin to get appropriate White Balance of my images.
After applying WB in Lightroom Temp is +11 and Tint is +91 (before it was 0,0).
Thing is how can this be applied in TI’s pipeline?

White balance matrix that I got in the code right now is set to: static int wb_table_def[] = {512,512,512,512,0,0,0,0};
which is being passed to the IPIPE driver with updateIpipeParam(wb_table_def, rgb1_table_def, rgb2_table_def) together with rgb2rgb matrices and here is how it is being used:
wb.gain_r.integer = U4_9_INT(wb_table[0]);
wb.gain_r.decimal = U4_9_DEC(wb_table[0]);
wb.gain_gr.integer = U4_9_INT(wb_table[1]);
wb.gain_gr.decimal = U4_9_DEC(wb_table[1]);
wb.gain_gb.integer = U4_9_INT(wb_table[2]);
wb.gain_gb.decimal = U4_9_DEC(wb_table[2]);
wb.gain_b.integer = U4_9_INT(wb_table[3]);
wb.gain_b.decimal = U4_9_DEC(wb_table[3]);
wb.ofst_r = wb_table[4];
wb.ofst_gr = wb_table[5];
wb.ofst_gb = wb_table[6];
wb.ofst_b = wb_table[7];

So, how should Temp and Tint be used to populate wb_table_def?

Thanks,
Teo