In Section 6.9 TCP2 Input Configuration Register 6, all the Tail Symbol Patters are identified as CDMA-2000. I think some of them should be identified as 3GPP. This also applies to Sections 6.10 - 6.14.
In Section 6.11 TCP2 Input Configuration Register 8, the description is missing for CDMA-2000 Tail Symbol Pattern for Code Rate 1/3, 1/2, or 3/4.