This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

android 2.3.4 play video on DM8148 with LCD panel

I am running android 2.3.4 on dm8148 board with LCD panel. I can not see the video when I play back video file. The following are the error messages. It seems that the driver can not use scaler to scale the video.  There is no problem to play video to HDMI output. 

Here is the video node I am using.  

echo vcompmux:dvo2 > /sys/devices/platform/vpss/video0/nodes

t81xx_vidout t81xx_vidout: VIDOUT0: setup failed enable=0 width=1920
height=1080 color_mode=1
pix_width = 1920 pix_height=1080 pos=0x0 out_width=800 out_height=480 screen_wid
th=3840
t81xx_vidout t81xx_vidout: VIDOUT0: apply_changes failed