This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

initrd not working with kernel of PSP 3.21.00.04

Other Parts Discussed in Thread: PCA9543A

hi

I was working with PSP 3.20.00.13 and the kernel was able to comeup with the ramdisk

my bootargs were :bootargs "mem=32M console=ttyS1,115200n8 root=/dev/ram0 rw initrd=0xc1180000,4M ip=off " 

now i have changed to PSP 3.21.00.04 and using the same boot args,

the kernel is panic  with no init found.

do i have to change the bootargs . TIA 

i2c-gpio i2c-gpio.1: using pins 20 (SDA) and 21 (SCL)
vpif vpif: vpif probe success
Switching to clocksource timer0_1
Unpacking initramfs...
Initramfs unpacking failed: no cpio magic
Freeing initrd memory: 4096K
EMAC: MII PHY configured, RMII PHY will not be functional
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 58
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a AR7
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a AR7
console [ttyS1] enabled
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a AR7
spi_davinci spi_davinci.1: DMA: supported
spi_davinci spi_davinci.1: DMA: RX channel: 18, TX channel: 19, event queue: 0
m25p80 spi1.0: m25p64 (8192 Kbytes)
Creating 6 MTD partitions on "m25p80":
0x000000000000-0x000000010000 : "UBL"
0x000000010000-0x000000090000 : "U-Boot"
0x000000090000-0x0000000a0000 : "U-Boot-Env"
0x0000000a0000-0x000000320000 : "Kernel"
0x000000320000-0x000000720000 : "Filesystem"
0x0000007f0000-0x000000800000 : "MAC-Address"
Read MAC addr from SPI Flash: ff:ff:ff:ff:ff:ff
spi_davinci spi_davinci.1: Controller at 0xfef0e000
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
i2c /dev entries driver
Linux video capture interface: v2.00
da850evm_enable_pca9543a
vpif_capture: could not setupinput for mt9t031
vpif_capture: probe of vpif_capture failed with error -14
watchdog watchdog: heartbeat 60 sec
cpuidle: using governor ladder
cpuidle: using governor menu
deviceless supply cvdd not found, using dummy regulator
omap_rtc omap_rtc: hctosys: invalid date/time
Freeing init memory: 88K
Failed to execute noinitrd.  Attempting defaults...
Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
Backtrace:
[<c00225fc>] (dump_backtrace+0x0/0x114) from [<c0181584>] (dump_stack+0x18/0x1c)
 r7:00000013 r6:c0035d10 r5:c00083ac r4:c025f170
[<c018156c>] (dump_stack+0x0/0x1c) from [<c0181600>] (panic+0x78/0x19c)
[<c0181588>] (panic+0x0/0x19c) from [<c001e5c4>] (init_post+0xa4/0xc4)
 r3:c1837c00 r2:00000000 r1:c02b0054 r0:c020ff8d
[<c001e520>] (init_post+0x0/0xc4) from [<c00084c4>] (kernel_init+0x118/0x154)
 r5:c00083ac r4:c025eba0
[<c00083ac>] (kernel_init+0x0/0x154) from [<c0035d10>] (do_exit+0x0/0x6cc)
 r5:c00083ac r4:00000000