We are using BeagleBone and the original Arago distribution (ti-sdk-am335x-evm-05.03.00.00). On certain Win7 machines when connected via usb, the BeagleBone will hang. Newer Lenovos show the problem, while older Dells do not. We've tried with various RNDIS drivers including those distributed with BONE_DRV and BONE_D64.exe, and the generic Microsoft Corporation RNDIS driver. Merely having the usb connected causes the problem, no actual ssh connection or anything needs to be active. Does anyone know why this would be happening? Is there a problem with the usb driver that is fixed in newer versions of the Arago dist?
Thanks