Hello all,
Before I proceed, let it be known that I am a complete novice when it comes to CCS 5 and TI products in general.
We have recently acquired a C6678 DSP, and we wish to run several benchmarks and tests on it. Specifically, we wish to analyze the cache, and ultimately we want to modify the cache. When it comes to the analysis part, we found information about a plugin called CacheTune; however, the information was about an earlier version of CCS, CCS 3, and we have not found a way to install it in CCS 5. Is there a way to install CacheTune in CCS 5? And if not, is there some similar tool that we can use?
We are aware of the Cache view under the Debug directory, but we need more information than that displayed in the Cache view.
Here is some additional information:
CacheTune manual: http://www.ti.com/lit/an/spraa01/spraa01.pdf
Board: TMS320C6678L
Sys BIOS 6.31.04.27
XDCtools 3.20.08.88
I will provide additional information if needed.
Thank you very much in advance.