Other Parts Discussed in Thread: TVP7002
I want to get a video from bt.601 camera and encode it to h.264 in real time. But,
i am stuck in getting video, the first step..
Some said ISS components needed, which local TI refuse to give whether NDA
is signed or not. They just said such modules are not available.
If it is possible to get a video, i will try connecting camera to output pins of tvp7002
(isolating tvp7002 outputs). But is there software component ready for this kind of try ?
In the similar post (http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/137058.aspx)
i see that Steve from TI said
"Does the camera output ITU656, ITU1120, RAW, some other format etc..
If the camera outputs ITU656 or ITU1120, or video data in YUV or RGB format then it can be connected to the VIn port.
If the camera outputs raw sensor data which needs to be processed through Bayer interpolation then the camera port can be used."
Then, is it possible bt.601 camera to be connected to Vin port, too ? How ?